Arrow Electronic Components Online

Barracuda vehicular 6 port antenna

Antennas12 Jul 2022
Truck on rural road with digital overlay showing sensor technology
View all articles

The public safety, transportation, and aftermarket fleet applications are dependent on rugged, high-quality RF communications gear. In this article, explore how TE Connectivity’s Barracuda RF antenna is a great fit.

Introducing the Barracuda antenna

The TE Connectivity Barracuda antenna is a ruggedly reliable, low-profile, multiport/multiband, 5G-ready antenna that provides an exceptional solution for today’s high-tech fleet applications. It can turn vehicles into communication hubs configured for ESN and FirstNet operation.

Multiport configuration

The Barracuda features six ports that are configured for the following:

  • Two-port MIMO operation over the 3G/4G/5G/ISM/CBRS bands

  • Two-port MIMO operation over the low/high-frequency Wi-Fi bands including Wi-Fi 6E

  • Fifth port – Has options for a third Wi-Fi, UHF, or future VHF

  • Sixth port – An additional port that provides an active antenna for enabling GNSS global navigation services

Key features

  • 5G ready

  • Low profile

  • Configured for ESN and FirstNet operation

  • IP67-rated, low profile, aerodynamic housing

  • Multiband/MIMO operation with GNSS navigation

  • Five-year product warranty

For further information, click through to the article.

Article Tags

Article
Global
Isolation