Arrow Electronic Components Online

Designing reliable and safe mobile robots with MCX’s error correction features

Macchine autonome11 ott 2024
L'immagine mostra robot autonomi che trasportano pacchi in un ambiente di magazzino moderno.
Visualizza tutti gli articoli

Truly autonomous mobile robots used to be science fiction, but recent advancements in processing, sensing and control have brought them closer to reality. One major hurdle facing this technology, though, is the ability for robots to self-correct if an error occurs in their processing operations. This article explores how MCX MCUs from NXP have advanced error correction features that make mobile robots safer and more reliable.

I robot mobili sono sempre più utilizzati in una vasta gamma di applicazioni, dall'automazione industriale alla robotica di servizio. Garantire il loro funzionamento affidabile e sicuro è fondamentale poiché questi robot svolgono compiti più complessi e operano in ambienti non controllati.

NXP's new MCX portfolio of microcontrollers help address these challenges. Built on the high-performance Arm® Cortex®-M33 core, MCX MCUs incorporate advanced error detection and correction features, making them well-suited for developing mobile robots requiring high reliability and safety levels.

Principali problemi di affidabilità e sicurezza nei robot mobili

Mobile robots rely heavily on their onboard electronics to perceive their environment, make decisions and control their actions. However, their operating conditions can be challenging due to various factors such as temperature extremes, vibration and electromagnetic interference. These stressors can cause bit errors and corruption in the robot's memory over time. Therefore, we need to consider the long-term reliability of the electronics, as mobile robots are expected to have long operational lifespans.

A group of autonomous robots designed for warehouse operations is seen navigating a polished industrial floor

AMR industriali

Figura 1

Memory errors can lead to various reliability and safety issues in mobile robots. A bit-flip in the robot's control firmware could cause it to execute incorrect instructions, leading to unintended behaviors. Corrupted sensor data could be misinterpreted, causing the robot to make incorrect decisions. Erroneous motor control outputs could result in unexpected motion or potentially damage the robot or its surroundings.

In safety-critical applications such as mobile robots operating near people, the consequences of such malfunctions could be substantial. Mobile robots need robust safeguards against memory errors to ensure reliable and safe operation.

MCX error correction features for flash and RAM

The NXP MCX A microcontroller series incorporates several key features to detect and correct memory errors. The MCX A embeds up to 128KB of flash memory with error correction coding (ECC) capabilities. The MCX N series features up to 2MB of flash memory with ECC. Each 128-bit word of flash incorporates an additional 9 bits of ECC data.

ECC is a technique of storing redundant bits with each data word. These redundant bits help to check the data integrity by regenerating the ECC bits and comparing them with the stored ECC on every read operation. If the regenerated and stored ECC bits mismatch, it means there is an error, which ECC may be able to correct. ECC can also determine which bit is erroneous in case of a single-bit error. However, it can only detect the double-bit errors but not correct them.

A sleek, modern robot with a white and black design is seen on a paved pathway in a park-like setting

Esempio di robot mobile

Figura 2

If the microcontroller detects an ECC error, the System Controller (SYSCON) module can generate a bus fault or use an interrupt to handle the error. Flexible fault handling allows developers to customize their handling to best suit their applications.

The MCX A also provides 32KB of on-chip SRAM, with an 8KB block (RAMA0) incorporating ECC for single-error correction and double-error detection. The MCX N series provides up to 416KB of RAM when configured as ECC, of which 32KB can be retained in VBAT mode. This feature protects critical runtime data, such as sensor inputs and algorithm state variables. The microcontroller implements an Error Reporting Module (ERM) to provide comprehensive reporting and control over errors. The ERM captures and logs error events from the ECC logic, providing visibility into the health of the memory subsystem. Developers can utilize this error information for diagnostics and predictive maintenance.

For self-diagnostics, the Error Injection Module (EIM) provides capabilities to inject errors when reading ECC RAM. This self-test feature allows developers to implement periodic self-checks to ensure the microcontroller operates reliably.

Oltre alla ECC, la serie MCX A include un Memory Block Checker (MBC) che fornisce un controllo di sicurezza runtime sui permessi di lettura, scrittura ed esecuzione per diverse regioni di memoria. Definendo politiche di accesso alla memoria, l'MBC può prevenire accessi non autorizzati alla memoria.

How MCX error correction enables reliable robotics

The MCX's error correction features work together to improve mobile robot reliability and safety. By automatically correcting single-bit errors in flash memory, the MCX maintains the integrity of the robot's control firmware. This integrity prevents the robot from executing erroneous control logic that could lead to unintended behaviors.

The MCX is equipped to detect double-bit errors, which is crucial for ensuring the safety and reliability of its operations. While it is not possible to correct double-bit errors, detecting them helps prevent the use of corrupted instructions or data. When a double-bit error is detected, the robot can be gracefully put into a safe state, thus avoiding potential hazards or malfunctions.

The MCX's ECC extends its memory protection capabilities beyond flash to cover SRAM. The MCX A’s 8KB RAMA0 SRAM block incorporates ECC, while the MCX N can repurpose RAMG and RAMH for ECC correction, providing up to 416KB of ECC RAM. ECC RAM enables single-bit error correction and double-bit error detection for runtime data. This functionality safeguards critical data such as sensor readings, control outputs and intermediate algorithm variables from accumulating single-bit errors that could otherwise cause inconsistencies in the robot's perception, planning and control logic. By maintaining the integrity of this runtime data, the MCX's SRAM ECC helps ensure the robot's situational awareness and decision-making remain accurate and reliable. The MCX N additionally provides up to 32KB of ECC RAM which can be retained in VBAT mode, allowing for data to remain protected while in a low-power state.

L'MBC fornisce un ulteriore livello di sicurezza applicando politiche di protezione della memoria. Può bloccare l'accesso non autorizzato alla memoria, aiutando a contenere i guasti e impedendo loro di causare comportamenti incontrollati del robot.

Finally, the ERM enables a data-driven approach to robot maintenance. By logging memory error events, the ERM provides visibility into the health of the robot's electronics. An increasing rate of corrected errors could indicate an impending failure, allowing the robot to be serviced proactively.

Esempio di caso d'uso

Considera un robot di servizio mobile che opera in un ambiente industriale. Il robot deve navigare autonomamente, evitando ostacoli e persone mentre esegue compiti.

A compact autonomous delivery robot navigates a busy city street at night

Robot di servizio mobile

Figura 3

However, the industrial environment can be challenging, with equipment generating electromagnetic interference (EMI). Over time, EMI could cause bit errors in the robot's memory.

The MCX's ECC would detect and correct any single-bit errors induced by EMI, ensuring the robot executes its control logic correctly. If a more severe double-bit error occurred, the MCX would detect it and prevent the use of the corrupted data. The robot could then initiate a safe shutdown.

Throughout these events, the MCX's ERM would log the error occurrences. Maintenance staff could monitor these logs, watching for any trends indicating a potential failure. By servicing the robot proactively, downtime is minimized and safety is maintained.

Esperienza per sviluppatori MCUXpresso

Per la prototipazione rapida con MCX, NXP offre la piattaforma di sviluppo FRDM a basso costo. Le schede di sviluppo FRDM sono dotate di fattore di forma standard e header, facile accesso agli I/O dell'MCU, debugger MCU-Link integrato e un cavo USB-C.

Il GitHub di NXP fornisce anche l'accesso a esempi di applicazioni, accessibili tramite il portale Application Code Hub (ACH). MCUXpresso IDE e MCUXpresso per VS Code hanno la navigazione ACH integrata, quindi gli sviluppatori possono facilmente cercare demo ed esempi disponibili e filtrare per dispositivo, tecnologia dell'applicazione o periferica/funzionalità prima di caricare direttamente il progetto per l'uso.

L'Expansion board hub (EBH) è un'estensione del sito SDK Builder di NXP, dove gli sviluppatori possono trovare una gamma di schede aggiuntive da NXP e partner per estendere le capacità della scheda di valutazione scelta. Questo hub offre un filtro intuitivo per trovare rapidamente le schede e individuare il software di supporto disponibile. Gli sviluppatori possono abbinare la loro scheda a diversi tipi di shield per valutare e fare prototipazione rapida per casi d'uso o applicazioni specifiche.

NXP consente la robotica mobile affidabile e sicura

As mobile robots become more autonomous, ensuring their reliable and safe operation is essential. If not addressed, memory errors induced by challenging operating environments can lead to unexpected robot behaviors.

NXP's MCX microcontroller portfolio is well-equipped to meet the needs of reliable robotics with its error correction features. From ECC-protected flash and SRAM to runtime memory access control and error event logging, the MCX provides multiple layers of protection against memory errors.

I progettisti di robot mobili che mirano a ottimizzare l'affidabilità e la sicurezza dovrebbero considerare l'NXP MCX. La sua architettura avanzata e il set di funzionalità completo lo rendono una piattaforma solida per sviluppare robot autonomi affidabili.

Servizi di Programmazione Dispositivi

Fornire servizi di programmazione di dispositivi di qualità su larga scala.

Tag articolo

Robotica
NXP Semiconductors
Macchine autonome
Automazione
Microcontrollers - MCUs

Articoli di notizie correlati

Mostra tutto