Advantages of MaxLinear UARTS & bridges: enabling seamless data communication

No matter how much data that customers in consumer, commercial, or industrial markets create, it’s useless without a way to interface with it and transfer it to other stakeholders. Therefore, receivers, transmitters, and other hardware are vital for data systems to reach their true potential. Read this article and learn how UART and bridge interface products from MaxLinear enable efficient data communications between wide-ranging devices.

In the ever-evolving landscape of technology, efficient data communication is paramount. MaxLinear has been at the forefront of developing cutting-edge UART (Universal Asynchronous Receiver/Transmitter) and Bridge Interface products that are revolutionizing data connectivity and bridging the gap between various communication interfaces. MaxLinear's UART and Bridge Interface products are paving the way for seamless and efficient data communication. With a focus on innovation, reliability, and security, MaxLinear is empowering industries, businesses, and individuals to embrace the full potential of connected devices and systems.

Unleashing Asynchronous Data Transfer

MaxLinear's UART solutions offer unparalleled reliability, enabling seamless and efficient data transfer without the need for a shared clock between the sender and receiver. The versatility of MaxLinear's UART products makes them ideal for a wide range of applications. From industrial automation to consumer electronics and Internet of Things (IoT) devices, UARTs bridge the communication divide, fostering interoperability and empowering devices to exchange critical information flawlessly.

Bridging Interfaces, Connecting Worlds: MaxLinear's Bridge Interface Product

In today's interconnected world, devices and systems often rely on different communication protocols, which can create challenges when trying to establish seamless connections. MaxLinear's Bridge Interface products come to the rescue by acting as intelligent translators, enabling efficient data exchange between disparate interfaces.

These Bridge Interface solutions support a variety of communication protocols, including UART, I2C (Inter-Integrated Circuit), SPI (Serial Peripheral Interface), and more. By converting data between these protocols, MaxLinear's Bridge Interface products break down communication barriers, enabling devices from different ecosystems to interact harmoniously.

Driving Efficiency and Innovation

MaxLinear's UART and Bridge Interface products are instrumental in driving efficiency and innovation across industries. In the industrial realm, these products facilitate real-time data transfer, ensuring smooth communication between machines and control systems. Manufacturers benefit from increased productivity and reduced downtime, ultimately leading to cost savings and improved operational efficiency.

The implementation of MaxLinear's UART and Bridge Interface products in IoT devices plays a pivotal role in creating a connected world. From smart cities to connected vehicles, these solutions empower IoT devices to communicate effortlessly, enabling data-driven decision-making and unlocking the full potential of the IoT revolution.

Security and Reliability: MaxLinear's Commitment

As data communication becomes increasingly critical, security and reliability are of utmost importance. MaxLinear understands these concerns and places a strong emphasis on ensuring the integrity of data transmission. Their UART and Bridge Interface products incorporate robust security features to safeguard against potential threats, providing peace of mind to users and businesses alike.

Moreover, MaxLinear's commitment to reliability ensures that their products can withstand demanding environments and extended operation. Whether it's in harsh industrial settings or mission-critical applications, users can trust MaxLinear's UART and Bridge Interface solutions to deliver exceptional performance without compromise.

MaxLinear UARTS & Bridges

XR21B1411IL16TR-F: Enhanced 1-CH Full-Speed USB UART

The XR21B1411 (B1411) is an enhanced Universal Asynchronous Receiver and Transmitter (UART) with a USB interface. The USB interface is fully compliant to Full Speed USB 2.0 specification that supports 12 Mbps USB data transfer rate. The USB interface also supports USB suspend, resume and remote wakeup operations.

Download datasheet

XR22800IL32TR-F: Hi-Speed USB to 10/100 Ethernet Bridge

The XR22800 is a Hi-Speed USB 2.0 compound device with an embedded hub and 3 downstream USB functions: 10/100 Ethernet MAC and PHY, multi-master capable I2C controller, and an Enhanced Dedicated GPIO Entity (EDGE) controller.

Download Datasheet

Featured Products

관련 상품 참조

XR21B1411IL16TR-F

MaxLinear, Inc USB Interface ICs 보기

관련 상품 참조

XR22800IL32TR-F

MaxLinear, Inc USB Interface ICs 보기


관련 뉴스 기사

2025 years ago

2025 years ago

2025 years ago

2025 years ago

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.