Differential current sensing with the 1 MHz bandwidth ACS733

This application note by Maxwell McNally from Allegro MicroSystems describes the use of the new highly isolated, high bandwidth ACS733 Hall-effect current sensor integrated circuit (IC) and gives an overview of its features and advantages over a highspeed current transformer (CT) current sensing solution.

Differential sensing

Current sensing technologies that depend on magnetic field for measurement can become compromised by external magnetic fields. By using two Hall plates measuring opposite polarities of the field created by the input current, the ACS733 is able to reject common-mode fields. This allows the part to be used near other current traces. The ACS733 has approximately –40 dB of common-mode field rejection for a uniform and constant field. For more information on differential sensing, see the application note “Common Mode Field Rejection in Coreless Hall-Effect Current Sensor ICs”.

The common-mode field rejection of the ACS733 is an advantage over a CT, because a CT core can saturate in the presence of external magnetic field and change the operating characteristics of the device.

Noise and sensitivity

The ACS733 has a typical noise density of 80 µA/√Hz. Across the entire bandwidth of 1 MHz, this becomes an input-referred total noise of 100 mARMS. At different sensitivities, this amperage error will manifest at the output as different levels of mV error, but this indicates the part has an effective 100 mA resolution. Table 1 below compares the mV output error seen for the currently offered sensitivities of the ACS733. However, this noise can be reduced by decreasing the effective bandwidth of the device, either with oversampling and averaging, or by filtering the output with an RC filter.

Table 1: Sensitivity and Resulting mV Noise

Allegro AN296154 Differential Current Sensing ACS733 Table 1

High bandwidth operation and fast response time

The ACS733 has a high operating bandwidth of 1 MHz. The device’s high speed analog signal path provides the fastest response time of any Allegro fully integrated current sensor IC. The typical response time to a step input is <800 ns on the output, and the typical fault output responds in <600 ns. Figure 1 shows the ACS733 responding to a current step compared to the response of a typical current transformer (CT). Both respond very quickly to the 1 µs input step.

Allegro AN296154 Differential Current Sensing ACS733 Figure 1
Figure 1: CT and ACS733 Step Response Comparison

User-settable overcurrent fault detection

An additional feature of the ACS733 is the user-settable overcurrent open-drain NMOS fault output. This allows an even faster reporting of overcurrent or shorting events. This pin will detect overcurrent events faster than ADC conversion of the analog output signal. The fault level of the ACS733 can be set to any level from 50% of the maximum primary sensing current (IPR(MAX)), all the way up to 200% of IPR(MAX) using a simple resistor divider on the VOC pin. This provides the customer an easy method to set the overcurrent level for their specific application.

The resistor divider on the VOC pin is set with levels of 10% of VCC to set the fault level to 50% of IPR(MAX), and a voltage level of 40% of VCC to set the fault level at 200% of IPR(MAX). Table 2 below shows these calculations for the ACS733 at four different fault levels. Equation 1 shows the calculation for the percent of VCC for any desired fault level.

VOCPercent = FaultPercent × 0.2 (1)

Allegro AN296154 Differential Current Sensing ACS733 Table 2

The fault signal is high when no fault is detected. When an overcurrent event occurs, the open-drain NMOS output pulls the output of the FAULT pin low. Figure 2 below shows the function of the fault output in response to a current step input. Since the device has an open-drain NMOS output, they can be logically OR’ed for multiphase systems to a single fault interrupt digital I/O pin of the controller.

Allegro AN296154 Differential Current Sensing ACS733 Figure 2
Figure 2: ACS733 Overcurrent Fault Detection

Compact Form Factor A current transformer is bulky, requiring an offset core with windings and a resistive load to sense current. The ACS733 is a fully integrated sensing solution in a standard SOIC16W surface mount package that takes up minimal printed circuit board (PCB) area. Below, Figure 3 shows the size of the ACS733 compared to two CTs. When trying to minimize the size of a system, the ability to run the current trace on the board to the part which is mounted to the PCB would offer a significant space-saving advantage.

Allegro AN296154 Differential Current Sensing ACS733 Figure 3
Figure 3: Size Comparison of ACS733 and Current Transformers

High voltage isolation

Despite its small size, the patented package technology provides for high-voltage isolation. The high-current pins are isolated from the low-voltage signal pins because only the magnetic field needs to be sensed. The ACS733 in the SOIC16W (LA package) is certified to 3600 VRMS in accordance with UL 60950-1 (edition 2).

Conclusion

The ACS733 has an array of features which offers significant advantages when high speed and high-voltage isolation current sensing are required. The LA SOICW package is a surface-mount solution that is easy to integrate and reduces PCB area over a bulky current transformer solution. The SOIC16 wide-body package of the ACS733 provides 3600 VRMS isolation from the current-carrying trace to the signal pins. The sensor IC is optimized over the operating temperature range at the Allegro factory and provides an open-drain NMOS FAULT output for a fast digital output when overcurrent and short-circuit events occur. This fully integrated sensing technology is truly a system-on-a-chip solution that is compatible with automotive and industrial applications, making it easy for engineers to design into their applications.

Download PDF

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.