How High did Whyachi Fly?

게시자

In one of the biggest hits in BattleBots history, Poison Arrow sent Son of Whyachi on a flight path across the battlebox.

Some speculate that Whyachi lost on a technicality due to not previously registering their 247lb drone with the FAA (though we have credible sources who say Whyachi’s radio receiver broke due to the impact). One of the most common questions we get asked is exactly how high did Whyachi fly through the air? Witnesses of the incident claim anywhere from 6 to 10ft.



With a little MythBusters style video sleuthing and high school physics, it’s pretty easy to calculate how high Whyachi flew. By replaying the video frame by frame, can see Whyachi spent a total of 1.1 seconds airborne. Summoning the powers of projectile motion, the vertical distance Whyachi traveled in that time can be found by:

Whyachi’s velocity Vo isn’t known at takeoff, but is known to be 0 at the apex of its parabolic trajectory. Since the time spent on ascent is the same as descent, the time should be divided by 2:

So about 5 ft, which is less than first hand witness accounts. We suspect that’s because folks based their live observation on “seeing the underside” of Whyachi, but upon replay it appears Whyachi had a slight tilt that caused it to flash its undercarriage only briefly. The fact Whyachi didn’t go tumbling through the air is a testament to how well its spinning hammers gyroscopically stabilized.

We’re not done analyzing the big hit yet though. It’s also possible to figure out how far horizontally Whyachi went by counting the number of steel floor panels which come stock in America at 4ft x 4ft, i.e. the bare minimum bed size of a proper American pickup truck:

We went ahead and highlighted the floor seams which required reviewing multiple frames of the video to identify. No single camera had a wide enough view to capture the entire flight which is why splashdown is off screen and had to be inferred by watching some of the other angles from the show.  The flight path looks to be 1.5 by 3.5 floor panels, or 6ft by 14ft. Going back to the classic 500BC Pythagorean theorem, Whyachi traveled the following distance: 

No matter how you slice it, the proof is in the math. That was one major hit.  



최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.