Network Connected Lighting for Commercial Buildings: Ready for A Breakout Year

Network connected lighting is beginning to transform the lighting industry—and the industries it serves. While the concept is already used in commercial buildings, its application is now spreading fast as large-scale projects get underway. Growing affordability and higher efficiencies are driving the use of network-connected lighting in commercial buildings, making possible concepts such as the smart building and other applications that drive efficiency and productivity. Innovative owners of enterprises and buildings are now perceiving network-connected lighting infrastructure as an asset that enables practical applications for the Internet of Things (IoT) and smart buildings and adds significant value to buildings and companies.

Growing Penetration

While still in an early stage, LED penetration in commercial buildings is reaching critical mass, making it cost competitive with other lighting technologies and enabling deeper market penetration.

Today, the use of LED technology in commercial buildings has moved past the innovation stage, where it had less than 1% share of the market, to the early adoption stage, where it now has about a 3% share, according to a 2015 study by the U.S. Department of Energy. Five years from now, the penetration of LED technology in the commercial building space is expected to be close to 25%. This growth pattern matches those of other lighting categories, such as traffic signals and exit signs, where LED penetration is now in the late majority phase, defined as 80 to 90% of the market, according to the study.

New Control Methods

The adoption of LED fixtures in commercial buildings is accelerating interest in network-connected lighting because more efficient and higher performance control makes it more affordable in commercial buildings. To date, the lighting industry has focused mostly on retrofitting existing lighting fixtures with LEDs to replace older technologies, such as fluorescent and compact fluorescent lighting. Controlled LED, however, not only improves efficiency but also provides better light quality, smoother intensity/dimming control, and dynamically adjustable color temperature, providing the right light when and where it is needed. This results in augmented worker comfort and more interactive and purposeful lighting and spaces for people. The ability to migrate lighting control to network IP-based infrastructure makes lighting a service and an IoT building asset that can be controlled synergistically along with other building functions.

It is important to note the difference between smart lighting and network-connected lighting. Smart lighting doesn’t necessarily need to be connected to a central network, and can be implemented simply by retrofitting older lighting fixtures with individual LEDs and sensors capable of simple, local control. Network-connected lighting, on the other hand, works with a centralized, software-based control system that coordinates all the elements in the lighting system, including luminaries, sensors, actuators and other devices. Lighting infrastructure is always present in a building and is very granular. More integration means not only better control but also more data and information being collected by a distributed sensor system as part of the lighting network.

Molex Network Conn Lighting_01

Figure 1: A schematic of Transcend®  Network Connected Lighting, a PoE lighting system. Transcend comprises software, networking technology, category cables, sensors, a PoE gateway, and lighting fixtures from various manufacturers

These data have the potential to open up new value propositions for commercial buildings. The first application is, of course, real-time energy usage reporting, but other applications—such as sensor-based occupancy reporting, light status and environmental monitoring—provide an entirely new view into how commercial buildings are used. By analyzing this data we will be able to know how many people are in the building at any given time, where they are located, how spaces are being utilized, the condition of those spaces and how usage of different areas of multi-floor and multi-building campuses compare to each other. All told, network-connected lighting will dramatically accelerate the integration of the IoT into commercial buildings.

New Deployments

New commercial buildings are the best candidates for network-connected lighting systems, which can be designed as part of a building’s infrastructure, but is suitable for deep-retrofit projects as well. There have been significant pilot installations of network-connected lighting in commercial buildings for some time, but 2016 saw larger-scale installations being integrated in buildings.

Not to be outdone by its own clients, Molex has installed network-connected lighting as part of a major retrofit of a building on its main campus in Lisle, Illinois. The multipurpose building, now called the “Vision Building,” is a showcase for PoE lighting technology and the possibilities it offers. The Vision Building, completed in the first half of 2016, is  a space where Transcend® Network Connected Lighting from Molex has been installed and is regularly demonstrated to guests. Transcend is a full-system network-connected lighting infrastructure primarily based on PoE power and data distribution. The Vision Building is a technology center and showcase for the entire Molex ecosystem of partners. The project demonstrates how commercially-ready network-connected lighting systems can improve lighting efficiency while also improving comfort, well-being and productivity. The retrofit also included a build-out of the “densification” concept, a change in interior building layout to include more offices in the same square footage in an open space layout while providing more shared space, including breakout and collaboration areas. Besides network-connected lighting systems, Molex and its partner companies provide new technologies in everything from IT network infrastructure to carpeting to washrooms.

Key Obstacles

While progress is being made in the deployment of network-connected lighting systems, several obstacles to deeper market penetration must be resolved. Today, traditional connected lighting systems are difficult to design and commission. Despite their many advantages, faster adoption of network-connected lighting systems requires that the installation, configuration and commissioning process these systems be simplified and standardized.

New Power Standards

Power over Ethernet (PoE) is one of the most promising technologies allowing IP convergence for building automation networks—including lighting—without the use of proprietary systems. LED technology requires low-voltage DC power in a different manner than older lighting sources, which utilize AC power that has been converted to low-voltage power. A smart network controlled LED lighting system requires only low-voltage power distribution and data communication for the control. Power and data on low-voltage cabling is possible using the same infrastructure that the IT industry has deployed for 15 years.

 

Molex Network Conn Lighting_02

Figure 2: Technology integrated within PoE lighting systems allows for full customization. End users can adjust lighting needs based on defined zones

PoE delivers electrical power over category cabling to networked devices and is widely deployed to provide power to various endpoints in commercial buildings, including VOIP, cameras, HVAC and now lighting. PoE offers high availability of power, guarantees uninterrupted service and lowers operating expenses by providing network resiliency at a lower cost by consolidating backup power. It also offers faster deployment of new networks by eliminating the need for a power outlet at every endpoint.

The driver of LED efficiency is its outstanding lighting output per watt of power, which far outstrips that of older lighting technologies. While already advanced, LED technology is becoming more versatile, efficient, secure and capable of supporting available wattages in network-connected lighting systems under the IEEE 820.3xx standard. This standard has been proven as a mechanism for classifying the endpoint devices needed to establish power connections.

For example, the original PoE standard IEEE802.3af, based on 15.4 w per switch port of power, has increased to 30 w in PoE+ (IEEE802.3at), the current standard. However, a new de-facto standard has been developed called UPOE, which delivers 60 w per switch port. The standard has now been succeeded by the Power over HDBaseT (POH) standard, which supports over 95 w per port. The IEEE is working to standardize the 60 w and 95 w PoE options under the 802.3bt specification, which is nearing completion now. The technology is backward-compatible and interoperable with the existing IEEE standard.

The 60 w and 95 w standards are based on using a four-pair power transfer format rather than the two-pair format used by the 30 w PoE+ standard. The new standards improve efficiency and allow a much wider range of device support while using the same low- voltage Class D (Cat5e) cable as the PoE+ standard.

In the existing PoE+ standard, a two-pair 30 w system delivers electrical power over two of the four available twisted pairs in Cat5e cabling. In this system, the pairs 1, 2 and 3, 6 are used to transport power from the PSE (power sourcing equipment) to the PD (powered device) and the spare pairs (4, 5 and 7, 8) are idle. The 60 w UPOE standard uses the same cabling as the 30 w PoE+ standard, but while the two-pair system uses one PSE controller to power the PD through the signal pairs of the cable, a four-pair system uses two PSE controllers to power both the signal pairs and the spare pairs. Because it uses all four twisted pairs to deliver power, UPOE can deliver more power and is more efficient than PoE+, reducing channel losses.

New Lighting Paradigm

Through the development of new products and new, more efficient standards, network-connected lighting is rapidly becoming a key part of commercial building design, and companies that create enabling technology for this new technology will help drive the industry through the transition.

Today, however, IT and lighting are still quite separate worlds. We need to create a bridge between these worlds, not only in terms of technology but also in the understanding of best practices for lighting architecture, construction, and installation, and best practices for the management, control and security of IT systems.

It is heartening to see that that is now beginning to happen. There are lighting manufacturers participating in IEEE standard committees, and IT companies participating in lighting standard committees. The Molex Transcend®  PoE Lighting System is a good example of how the IT world and the lighting/building automation world are merging. There is a transition occurring in the industry where lighting architects, electricians, MEPs (mechanical/electrical/ plumbing contractors), installers, and low-voltage power and data specialists are showing great enthusiasm for PoE connected lighting systems. On average, it is estimated that PoE network-connected lighting systems (and low-voltage lighting systems in general) offer between 10% and 25% capex savings compared to traditional line voltage LED lighting control systems.

Molex Network Conn Lighting_03

 

Figure 3: PoE lighting system modules (top right) allow lighting designers to implement a variety of lighting methods, including directed, indirect, ambient, and decorative

The potential advantages are great. Network-connected lighting can increase lighting efficiency up to 70% compared to traditional lighting control. But, as mentioned earlier, better and more effective lighting can also increase worker productivity, which can have a profound effect on company performance. For example, a 2012 study by the Rocky Mountain Institute found that the annual cost of energy in an average commercial building is about USD 3 per square foot (USD 30 per m2). The annual cost of a mortgage or rent on the building is about USD 30 per square foot and the annual cost of salaries for the people working in the building is about USD 300 per square foot (USD 3,000 per m2). That means if the productivity of the people working in the building can be increased 1%, it will produce annual savings of USD 3 per square foot, which would pay for the total cost of energy.

Studies show that better light and more natural light can fuel those improvements in productivity as well as improvements in health and well-being. The Center for Building Performance and Diagnostics at Carnegie Mellon University identified 12 studies linking improved lighting design with 1% to 23% gains in individual productivity. The studies measured productivity gains through increases in reading comprehension, letter processing speed and a range of other tasks, as well as reduced absenteeism.

Also, keep in mind that, as with any new technology, potential new benefits of network-connected lighting will likely emerge. As commercial buildings migrate to the IoT via IP protocols that open the door to big data analytics, the long-term significance of that development as part of the value proposition for network-connected lighting is just beginning to be understood.

molex logo

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.