MOSFETs - The Truth is in the Datasheet

게시자

In the world of electrical engineering, it’s important to realize that numbers can lie. This is especially true when looking at MOSFETs.

The first page of a datasheet is notorious for this because manufacturers often cherry pick numbers at specific test parameters to stack up well against the competition. The published parameters help us understand the basics of the part we're looking at, but rarely do they actually help us make a final decision on which part we need to use. To understand the parts better and make the best choice when it comes to the system you are creating it is well worth it to dive deeper into the specifics of the datasheet.

When sorting through the parametric data you might end up with 5 to 10 different parts that all seem to meet the needs of your system. All the parts seem equal in capabilities, so how do you make the right purchasing decision? This is where the world of the Safe Operating Area (SOA) becomes important. All of the parts you are looking at may claim to have the same voltage and amperage characteristics but when you dive deeper into the datasheet you may notice significant differences in their performance. I picked the SOA characteristic specifically for this article but there is a lot more you can find in the datasheet to help you choose the right part—like how Rds(on) can change over temp or how hard you need to drive the part for a specific set of current and voltage outputs.

What is the safe operating area? The SOA is a region defined by voltage and amperage telling you how long a part can survive operating under certain conditions without damaging itself. The SOA is based on a combination of factors from the type of substrate to how well the specific package can dissipate built up heat. For many MOSFETs it is incredibly rare to find one that will survive the maximum voltage and amperage rating listed on the datasheet at the same time for anything longer than a microsecond. Even a microsecond is often being generous. Usually a part will fail quickly at the top end of its operating range, where it’s only useful in bursts. There is also a burst or peak current at which a part can survive but this is distinct from an operating burst as it pertains to the SOA.

I want to look specifically at two different parts today. Both of these parts are 650 volt 32 amp MOSFETs. According to their datasheets, these parts should both be adequate for the same system. If we look at the SOA graphs for the same package type and at the same 100 volt rating, we can see how long they will survive if we put 10 amps through them. For the part on the left (STI40N65M2 from STMicroelectronics), if you follow the graph, you will see it is designed to survive for a little less than one millisecond. If you look at the part on the right (IPP60R099P6XKSA1 from Infineon), under the exact same conditions, you will see that it can survive 10 milliseconds. Both of these parts have the same specifications on the first page of their datasheets, but you can see that the part on the right will survive edge-case scenarios much better that the part on the left. It also happens to be $0.10 cheaper. It pays to delve into the statistics.

Part choices matter, so don’t be afraid to dive deeper into the datasheet to make sure you get the right one for your system. Going beyond the first page can make all the difference.


최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.