PoE is an ideal solution for smart building

Smart buildings need to connect in series many devices and systems including security monitoring, lighting, air conditioning, etc., involving complex data and power transmission wiring, so as to ensure the stable operation of the systems. Power over Ethernet (PoE) technology can transmit power and data to devices through twisted pair at the same time, so it can greatly reduce the complexity of system construction, reduce the cost of construction and improve the efficiency of operations. This article will show you the latest technology development of PoE and related product solutions launched by onsemi.

APAC-20211019-3002

PoE has technological advantages and the market development potential is amazing

After years of technical evolution, PoE has introduced three standards, which can be divided into IEE802.3af (15W), IEE802.3at (30W) and IEE802.3bt (90W) according to the supported power. PoE is used to supply power and transmit data for smart building application systems. Since manpower costs are not required, it has the advantages of easy installation, and reduced capital expenditure and operating costs.

For wired smart equipment (such as lighting, security devices, etc.), PoE technology can greatly reduce the complexity of system construction, and meet international safety standards. For certain equipment far away from the power outlet, such as Wi-Fi access points, Femtocells, Picocells, etc., PoE technology has more advantages, and can build centralized standby power supply (such as UPS), which can run continuously during power failure. The use of PoE technology will achieve great benefits.

Depending on the power supply mode, PoE can be divided into Power Sourcing Equipment (PSE) and Powered Device (PD), and the market is growing rapidly. According to the market analysis made by Global Markets Insights, taking the US market as an example, the PSE equipment of PoE in 2018 was USD 110 million, which is expected to grow to USD 300 million by 2025. PD equipment is expected to grow from USD 175 million in 2018 to USD 400 million in 2025. The market development potential is extremely amazing.

 

APAC-20211019-3003

Support higher power to meet more diverse application requirements

The IEEE802.3bt standard officially launched in October 2018 and adopts four pairs of power and can provide up to 90W, which further develops PoE applications by supporting more diverse devices, such as Smart Kiosks, POS, and cameras supporting 1080p, PTZ functions and heaters, or Wi-Fi routers supporting 802.11ax standards, LED lighting, TV/digital signage, and computers. It can be widely used in office spaces, residences, industrial applications, museums, universities, public education, government agencies, airports, corporate communications, health care, and other fields.

IEE802.3bt can transmit power on all four data connection lines (960mA/pair), support up to 90W power output, and support finer resolution classification, allowing PSE to better optimize power distribution among multiple PDs, and has backward compatibility. IEEE802.3bt also has the Maintain Power Signature (MPS) Function. When the MPS of PD does not exist for at least 400 milliseconds, the PSE will recognize the disconnected PD, and at the same time, the PD in sleep mode will generate pulse current (MPS) to avoid triggering the PSE to disconnect, and not consume too much power on the PD.

In addition, according to the National Fire Protection Association (NFPA), the third major cause of commercial fires in the United States is “electrical and lighting equipment”. Typical root causes include old or defective lines, circuit overload, loose connections, fuse failures, imbalanced electrical loads and many other electrical or lighting problems, which lead to overheating or sparks and may thus lead to fires.

The PoE standard transfers safety control from copper (power supply) to silicon (chips). On the one hand, silicon is much cheaper than copper; on the other hand, we can code silicon chip instead of copper. The equipment adopting PoE technology will be safer and more efficient than the traditional equipment using alternating current directly. However, such advantage of PoE over mains power is often overlooked.

APAC-20211019-3004

Highly integrated PoE-PD interface controller

For PoE applications, onsemi introduced NCP1095/NCP1096, a PoE-PD interface controller compliant to IEEE.3bt, IEEE 802.3af and/or IEEE 802.3at, which can realize the development of high-power applications such as connected lighting and security cameras, and ensure interoperability among PoE devices. NCP1095/NCP1096 combines all functions in one PoE system, such as detection, classification and current limiting in the inrush phase. NCP1095/NCP1096 uses external pass transistors to provide output voltages of up to 90W. NCP1095/NCP1096 has auxiliary detection pins for applications powered by PoE or wall adapters, and also provides automatic classification support for optimizing power distribution based on PD type and classification. It also provides internal hot-swap FET for higher level of integration (NCP1096).

NCP1095/NCP1096 can be applied to Power over Ethernet Powered Device (PoE-PD) and Internet of Things (IoT). The end products include digital signage, satellite data network, connected lighting, video and VOIP phones, security cameras, pico base stations, multi-band access points, USB Type-C devices, etc.

APAC-20211019-3005

In order to speed up the product development of customers, onsemi also introduced the NCP1095GEVB/NCP1096GEVB PoE-PD interface controller evaluation board, which can provide customers with the development and evaluation of NCP1095/NCP1096 controllers. The evaluation board also includes a RJ-45 connector, power transformer, active bridge (Greend Bridge2) and other fixtures to help end user with testing. It is the best evaluation tool for developing PoE applications.

APAC-20211019-3006

Intelligent LED driver supporting indoor positioning technology

Aiming for the intelligent lighting application of smart buildings, onsemi introduced NCL31000 intelligent LED driver, which is a device conforming to the technical specification of YellowDot™ indoor positioning, and has the functions of precise dimming, diagnosis and power measurement. NCL31000 integrates a high-efficiency efficient buck LED driver, supports high-bandwidth analog and PWM dimming to zero current, and also includes two auxiliary DC-DC converters. These are used to power the microcontroller and other sensors. Its built-in diagnostic function can measure input and output current and voltage, LED temperature, and DC-DC voltage. This device is very suitable for YellowDot™ LED driver. In addition, onsemi also introduced the reduced-feature version of NCL31001, which supports multi-channel solutions.

NCL31000 is a high-efficiency buck LED driver, which integrates a 3.3V buck converter, can adjust the voltage from 2.5 to 24V, has an I²C or SPI serial interface, has a high modulation bandwidth (~50kHz), supports Visible Light Communication (VLC), and can send signals to cameras on mobile phones or tablet. Each LED ballast has a unique identifier. When the camera of a mobile phone detects the code, it can indicate the position of the mobile phone in the building with an accuracy of less than 30cm.

NCL31000 can perform deep dimming to zero with an accuracy of 0.1%, support low EMI design, prevent LED short circuit and open circuit, and has IC and LED overtemperature protection, as well as diagnostic functions for measuring voltage and current. NCL 31000 can be used for LED lighting and backlit LED drivers. Common end products include YellowDot™ LED drivers and intelligent LED luminaries.

APAC-20211019-3007

onsemi also introduced the NCL31000ASGEVB evaluation board, an Arduino Shield evaluation board for the NCL31000 intelligent LED driver that supports VLC and compliant to YellowDot™ specifications. It has >97% overall solution efficiency, supports functions including EMC, DC-DC, diagnostics, realizes true dimming to zero with high linearity and 0.1% accuracy, with input voltage from 24 to 57V, LED power capability more than 100W, and an optional I²C/SPI interface (NCL31000MNITWG I²C variant can be mounted). It can be used in VLC, connected indoor and outdoor lighting, multi-channel managed lighting, theater lighting, therapeutic lighting, information displays, backlights, and hazardous or sensitive environments.

Conclusion

Smart building applications have gradually become an important trend in current architectural design, and PoE technology is an ideal solution for smart building applications. onsemi's PoE solution can support the latest IEEE.3bt standard and provide up to 90W power, which is an ideal solution for PoE-PD. With the NCL31000 intelligent LED driver, it can provide more convenient and efficient product development and application for intelligent lighting applications, which is worthy of in-depth understanding by manufacturers interested in entering smart building applications.

관련 상품 참조

NCP1095DB

onsemi Power Over Ethernet - PoEコントローラ 보기

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.