Power Factor Correction Basics

게시자

Power factor (PF) of an alternating current (AC) source is defined as the ratio of the real power (Watts) flowing into the load to the apparent power (VA) in the circuit

It is given as:

PF = Real Power (W)/Apparent Power (VA) 

The above equation shows that PF is a number that can vary between 0 and 1. PF is 1 when the real power and the apparent power are the same. This happens only when both the current and voltage waveforms are in phase and sinusoidal (Figure 1). However, if both are sinusoidal but out of phase, the apparent power is more than the real power, and PF is the Cosine of the phase angle θ between current and voltage waveforms. In other words, PF = Cosθ. In practice, PF = 1 is an ideal situation where the load is pure resistive and linear. In reality, off-line AC/DC power supplies found in electronic systems are switched-mode, presenting a nonlinear load.  


Figure 1: Power factor is 1 when both the input current and voltage waveforms are in phase and sinusoidal. (Source: Infineon)

Since power supplies today are primarily switched-mode, they draw a non-sinusoidal waveform, resulting in a phase angle θ between the input current and voltage waveforms. When the current waveform does not follow the voltage waveform (Figure 2), it results in a PF below 1 based on Cosθ. For instance, if θ = 45°, PF = Cos45 = 0.707. Besides power losses, < 1 PF causes harmonics that travel down the neutral line and disrupt other devices connected to the AC mains line. The lower the PF number, the higher are the harmonics content on the AC line, and vice versa.  


Figure 2: Power factor is below 1 when the current waveform does not follow the voltage waveform. (Source: Infineon)

Subsequently, there are stringent regulations to limit the harmonic distortion permitted on the AC mains line. A popular European regulation is EN61000-3-2, which was introduced to limit sending back reflected harmonics from electronic equipment into the mains. It is applicable to all Class D electronic systems, such as PCs (including notebooks and PC monitors), and radio and TV receivers consuming more than 75 W. Class D is one of the four classes (A, B, C, and D) categorized by the EN61000-3-2 standard, which imposes different harmonic-current limits on each class. It is now an international standard. 

To comply with the harmonic requirements of regulations like EN61000-3-2 and maintain high overall PF performance, it is necessary to incorporate power-factor correction (PFC) in the AC/DC front-end converter modules used in electronic systems consuming more than 75 W. Implementing PFC achieves a high PF number and ensures low harmonics. Today, there are a number of passive and active techniques available for numerous power-supply topologies employed in the AC front-ends.

Passive PFCs 

The simplest way to control the harmonic current is to use a passive filter comprising an inductor and a capacitor. By passing the current only at the line frequency (e.g., 50 or 60 Hz), this LC filter reduces harmonics, enabling the nonlinear device to look like a linear load; thus, helping the PF to approach near unity. However, the drawback is that the filter requires a large-value high-current inductor and a high-voltage capacitor, which is bulky and expensive.

Active PFCs 


Figure 3: The active PFC solution uses a semiconductor controller, which is placed between the input rectifier and the storage capacitor, followed by the DC/DC converter.  (Source: ON Semiconductor)

The active PFC solution uses a semiconductor controller chip, which is placed between the input rectifier and the storage capacitor, followed by the DC/DC converter, as shown in Figure 3. This circuitry shapes the input current to match the input voltage waveform and achieve a high value of PF, normally above 0.9. Fundamentally, there are three different types of active PFC controller ICs. These include critical-conduction mode (CrM), continuous-conduction mode (CCM), and discontinuous-conduction mode (DCM). There are several manufacturers offering a variety of these active PFC controller ICs, with each supplier offering its own versions along with the rationale for using them. 

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.