Product Roundup – RF Diodes

게시자

RF diodes are a key part of RF circuits. These diodes are tasked with handling high-power RF signals in such applications as RF and microwave devices, TV monitors, radio transmitters and stereo amplifiers. A diode is asymmetric in its transfer so that there is a low resistance to current flow in one direction and a high resistance in the opposite direction. There are several types of RF diodes, including:

  • PIN diodes that, when forward-biased, are linear and behave like a resistor. They are effectively used as a variable resistor in a variable attenuator and also used as an RF switch. In a forward direction and sufficiently biased, it has a low resistance to the RF that needs to be passed. In comparison, when a reverse bias is applied, it acts as an open circuit, yielding a relatively small level of capacitance. Applications include antenna switching for cordless and cell phones, band switching for tuners, RF attenuation and overvoltage protection. PIN diodes are also used in RF protection circuits to protect a sensitive receiver from the effects of a large transmitter when placed across the receiver input. PIN diodes also have many applications as photodiodes.

 

Figure 1: An RF diode schematic diagram. (Source: General Microwave)

 

  • Schottky diodes have a metal to semiconductor contact. They are used in high-frequency and fast-switching applications such as voltage clamping or to avoid transistor saturation. Examples include the RF081L2STE25 Schottky diode from Rohm. The diode’s temperature range is -55°C to 150°C. It has a peak reverse current of 10 uA, peak reverse repetitive voltage of 200 V, maximum continuous forward current of 1.1 A, peak reverse recovery time of 25 ns and peak forward voltage of 0.98 V at 1.1 A. It is a 2-pin surface-mount device with a J-Lead shape. Another Schottky example is the CDB7619-000 RF diode by Skyworks Solutions. The surface-mount device is used in such applications as detectors and mixers. The beam-lead and chip Schottky barrier detector diodes are used in applications through 40 GHz in the Ka band. The manufacturing process and materials yield low series resistance and a narrow spread of capacitance values for close impedance control. N-type silicon is also available.  Mounted beam-lead diodes are ideal for use in waveguide, coaxial, and stripline applications, while unmounted are suited for use in Microwave Integrated Circuit (MIC) applications.
  • Other types include varicap, a.k.a. varactor diodes, used in voltage-controller capacitors so that tuning circuits such as TV receivers lock fast. In this and other uses, they eliminate moving parts.

 

  • Impact ionization avalanche transit-time (IMPATT) diodes operate at very high frequencies and are used as elements in RF/microwave devices, while tunnel and Gunn diodes are used in oscillators and other RF apps.

 

  • Also available is TE Connectivity’s RF2524-000 ESD Suppressor Diode Arrays. A member of the SESD series of ultra-low capacitance diode arrays, it provides signal integrity while preserving unidirectional ESD protection of high-speed serial interfaces. There are several packaging options ranging from the standard 2.5 mm x1.0 mm layout to a 0802 and 1103 DFN that minimizes trace layout complexity and saves PCB space. There is more than 20 kV contact ESD protection (IEC61000-4-2) combined with extremely low leakage and dynamic resistance. Applications include USB 3.1, 3.0 and 2.0, HDMI 2.0, 1.4a, 1.3, DisplayPort, V-by-One, Thunderbolt (Light Peak), LVDS interfaces and applications in consumer, mobile, portable electronics that need high ESD performance but are housed in a small package.

 

 

 

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.