Protection Against Thermal Runaway

A thermal runaway is an increasing threat to electronic devices where more and more power is packed in ever smaller spaces; it is a threat that is poorly dealt with using traditional means. SMD thermal fuses offer a solution that can be reflow-soldered at 260°C and still open at 210°C.

What is meant by a thermal runaway or the thermal damage of power semiconductors: A thermal runaway refers to the overheating of a technical apparatus due to a self-reinforcing process that generates heat. This damage usually causes the destruction of the apparatus and often leads to a fire or explosion.

Causes

The causes of a thermal runaway are varied and often random in nature. However, the ever-higher power density in electronic wiring and the trend towards miniaturization are without a doubt of particular importance. More and more functions are packed in compact modules, which then also have a correspondingly high power consumption.

Even slightly excessive currents in power electronics with only a little power loss lead to elevated temperatures of approximately 200°C.

The possible consequences: damage or disconnection of surrounding components, damage to the printed circuit board structure or, in the worst case, the triggering of a fire.

Build up

With a power semiconductor (e.g. MOSFET) the drain-source transmission resistance increases with rising temperatures, when connected, which results in an increasing loss of power in the barrier layer. If the elements are not sufficiently cooled - the high power density permits cooling - the power loss output in the form of heat can no longer be sufficiently dissipated, which also increases the transmission resistance. This process escalates and ultimately leads to destruction of the component.

ThermalRunaway_2

Cause diagram for thermal runaway at an n-channel MOSFET 

How to protect against a short circuit?

The cooling of a system must dissipate at least as much energy as it is supplied with. The overcurrent during a thermal runaway is too low to cause a conventional fuse to trip. Thermal circuit breakers or PTCs would, in principle, be used, but the products available for the assembly of an SMD printed circuit board are too complicated or completely unsuitable.

Solution

SCHURTER develops and manufactures SMD thermal fuses with the lowest possible internal resistance for power electronics of the highest packing density. They can be reflow-soldered at a maximum temperature of 260°C without opening. The temperature trigger is therefore around 210°C during operation. This corresponds to a range above normal component temperature ratings, but still below the limit to create serious consequences,The fuse opens with or without current flow depending on the temperature. Such irreversible thermal fuses are resistant to mechanical shock, vibration, thermal shock, temperature cycles and moisture. They are qualified according to AEC-Q200. 

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.