Stop! Shunt Regulators Help Your Car Come to a Halt

게시자

Shunt regulators can play a key role in dynamic braking systems, which are commonly used to decelerate electrically-powered vehicles.

The shunt regulator is a type of linear regulator, a system used to maintain a steady voltage in an electrical circuit. In a linear regulator, the level of resistance changes to accommodate the input, producing an output voltage that is constant. The regulator dissipates the difference between the input and output voltages in the form of waste heat.

Linear regulators sometimes are placed between the source and regulated loads. These are called series regulators. In contrast, shunt regulators are placed in parallel with the load.

Shunt regulators can be very simple in design, with some consisting of a single reference diode. They are commonly used in voltage reference circuits and DC power supplies.

Using shunt regulators, designers can control the voltages on their systems to prevent shutdown and component burnout.

Shunt Understanding

Suppliers of shunt regulators include Microchip Technology Inc., Texas Instruments, Fairchild Semiconductor, ON Semiconductor, NXP Semiconductors, and more.

Beyond dynamic braking, there are multiple applications for shunt regulators including:

  • Error amplifiers
  • Independent source circuits
  • Precision current limiters
  • Precision voltage references
  • Switching power supplies
  • Voltage supervision and monitoring


관련 상품 참조

SR10LG-G

Microchip Technology Special Purpose Voltage Regulators 보기


Step on the Brakes

Dynamic braking is defined as using the electric traction motor of a vehicle as a generator in order to decelerate. In such a system, the electric motor runs backwards to slow the vehicle.
This brings into play a fundamental truth about electrical generation—when motors run forward, they produce motion; when they run backwards, they become generators and make electricity. Thus, dynamic braking transforms the energy used to slow down a vehicle into electricity.
This system brings several benefits, including lowering the wear on friction-based braking components.

Electricity Excess

However, dynamic braking raises an important question. What is to be done with the electricity produced by the motor or generator?

One approach to dynamic braking is known as rheostatic. For rheostatic braking systems used in locomotives, the energy generated by running the motor backwards is dissipated as heat by a resistor. Large train diesel engines use arrays of resistors and large cooling fans to prevent overheating.

This is a relatively inexpensive approach to dynamic braking, although it wastes the energy produced by the system.

관련 상품 참조

TLV431AQFTA

Diodes Incorporated Voltage References 보기


Talkin’ ‘bout Regeneration

Another approach is to use regenerative braking, which is a system used in some hybrid automobiles such as the Toyota Prius. In regenerative systems, the electricity is sent back into the system in order to charge up the batteries.

This is the most efficient approach to dynamic braking, ensuring that more of the electricity produced is used to propel the vehicle. On the downside, regenerative braking is a more expensive way to implement braking compared to the rheostatic approach. However, despite this additional cost, hybrid vehicles use regenerative braking as their primary means of deceleration.

Some cars using conventional internal combustion engines are employing regenerative systems to power electrical components in the car. For example, Mazda’s i-ELOOP system uses a regenerative braking system to charge supercapacitors that, in turn, supply electricity for the electronic equipment.

Feel the Burn

For either approach, the electricity generated by the motor or generator needs to go somewhere. For regenerative systems, this electricity feeds back into the batteries.

In the rheostatic approach, as the motor runs backwards, the voltage on the DC bus of the motor control will start to increase. This could cause a shutdown or component burn out among components connected to the motor’s bus. To protect their circuits, designers must devise a way to deal with this voltage.

One solution is to employ a shunt regulator that consists of a resistor and a voltage regulated switching transistor. Such a shunt regulator dissipates the voltage as heat.

Accelerated Braking

With the use of electrical motors in a variety of systems, dynamic braking systems employing shunt regulators are likely to be prevalent.

 

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.