What is I/O? Understanding GPIO & Input/Output Functions

I/O is one of those concepts that can seem self-explanatory. But simple as they may seem, inputs and outputs are a building block of modern electronics.

Inputs and outputs are fundamental to the world of computing (and more generally in data/information processing). Without them, electronic devices of all kinds would have no way of receiving data, and the user would have no way of manipulating or interacting with that data. Since they form the basis of our relationship with almost all the devices we use, it’s important to understand how inputs and outputs function.

What is Input and Output?

Simply put, inputs and outputs are the ways that a computer (or another device) interacts with the world.

Inputs refer to any way that the computer receives data from outside world. The most obvious examples are your computer’s keyboard, trackpad, or mouse, but “inputs” can also include cameras, microphones, and other devices or systems that supply data to a given computer.

Outputs operate similarly, but in reverse. Outputs enable computers to address the physical world; these devices include displays and speakers, but also controls and signals for tasks like turning lights off and on, controlling motors, and more.

How Computer Input and Output Works

Generally, I/O devices communicate with a computer through an interface called a bus. This interface has two main functions.

1. Interpreting. The bus addresses and performs “handshaking” between the devices using basic commands (like “READY” or “BUSY”). This handshaking allows the devices to communicate with each other successfully.

2. Converting. The interface’s second function is to convert data from serial to parallel or vice versa when necessary. This conversion is what allows devices with different types of information to communicate.

Computers and most other digital systems operate in binary, so any input signal must be in binary by the time it arrives at the computer’s processor. Therefore, any analog inputs go through a conversion to digital using an analog-to-digital converter (ADC) – though that is often part of the device/peripheral itself, as in the case of a scanner. The digital signal that results may also need conversion, as mentioned above, since digital data can be either serial or parallel. At this stage, the bus can typically facilitate conversion between types of digital data.

Conversely, an output bus will facilitate the conversion of the computer’s data into whatever form is needed, whether it’s audio, video, or something else. In some cases, such as with audio, digital information will convert back into analog. Users will need to employ a digital-to-analog converter (DAC) to allow the data to be used with real-world devices.

What is GPIO?

A general-purpose input/output (GPIO) is a digital data pin on a circuit (either an integrated circuit or electronic circuit board). A user may change the GPIO’s function at run time and manipulate the pins to operate as inputs or outputs.

Most GPIOs cannot output enough current to power devices like lightbulbs or motors on their own. To use a GPIO to control such a device, you’ll typically need to use a transistor and/or relay to directly power it.

Input and Output Summary

I/O is a broad term that encompasses many different types of auxiliary devices. It is also the concept that governs how humans interact with computers and how computers interact with the world around them. A basic understanding of inputs and outputs can help you approach device construction and manipulation more efficiently and precisely.

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.