Current in Termination Resistors in Case of Short Circuit to Vbat Using TLE6250G and TLE6251G High Speed CAN Transceiver
Infineon Technologies AG이 부품 TLE6251G 을 사용하는 참조 설계
이미지
1 / 1
최종 제품의 경우
- Automotive Environment
- Infotainment System
Description
- Current in Termination Resistors in Case of Short Circuit to VBATT Using TLE6250G and TLE6251G High Speed CAN Transceiver. It shows the path of the current, in the case the termination is splitted (2x60 or 120) Ohm. The transceiver will limit the current to the ICANL_SC value, if the battery voltage is higher than 12V