Innovative ways to apply Arduino for industrial use

게시자

The Arduino Uno R3 from Arduino is one of the most popular microcontrollers out there, and it boasts a large online community that has created thousands of projects. Whether you want to monitor temperature and humidity outside your house or have the Arduino control a robot to auto-balance itself, the Arduino has a versatile set that can be applied in many DIY applications. But how does Arduino work in industrial solutions?

The industrial industry

For the industrial industry, the most common computing devices to control automation and other factors are PLCs (Programmable Logic Controllers). These are usually heavy duty and are made for use in manufacturing plants. If you’re hoping an Arduino Uno can replace the PLC that most manufacturing process centers use, you’ll be out of luck. There is a reason why PLCs (which can be hundreds of dollars) are more expensive than Arduino boards (about $20 - $30).

PLCs are different from other computing devices as they are intended for severe conditions found in manufacturing plants. This means they can handle dust, higher and lower temperature, and moisture—environmental conditions the Arduino isn’t built to handle.

PLCs also have more extensive input/outputs (I/O) to connect to other sensors and actuators. A PLC can output to other elements, including electric motors, magnetic relays, sirens, indicator lamps, and much more. This is something that the Arduino can also do, but it is more limited, as its analog inputs are only ranged from 0-5 V and the analog outputs are pulse-width modulation (PWM).

1117_Arduino_Industrial_Solutions
The Arduino Uno.

Arduino for industrial use

While PLCs are the go-to for the Industrial Industry, that doesn’t mean there are no Arduino industrial applications. One task that Arduino is great for is collecting data, so if you need to collect temperature and humidity, you can easily insert the Arduino to monitor many variables. This will give you a chance to check if there are any problems with the machinery. Think of it as an added set of eyes for all types of machinery.

If we are talking about smaller scale industrial solutions, like having an automated sprinkler system in your house, then the Arduino is perfect for those DIY projects. The Arduino sensors and its wide variety of shields can be used to create DIY solutions at home that include building digital dashboards with important information, monitoring crops, monitoring water flow, creating a control center, or even building an automated irrigation system.

The Arduino is great for small-form solutions that you can build yourself at home, but it can also be utilized on large-scale projects when used to keep track of data and processes. Additionally, the online Arduino community is one of the strongest out there. You’ll be able to find different ways you can apply your Arduino in variety of solutions.


관련 상품 참조

A000066 | Arduino Uno Rev3

Arduino Corporation Embedded System Development Boards and Kits 보기


최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.