Fiber-Optic Adapters Help Systems Communicate

게시자

Fiber-optic systems date back to the early 1970s, and multiple connector types have come and gone since then, ranging from the early Deusch 1000 (perhaps the first commercially successful connector) to the current miniature LC type.

Along the way, performance has improved, too.  The Deutsch 1000 achieved about 3 dB insertion loss, compared to 0.25 dB for the LC connector.


Figure 1:  Fiber-optic connectors (newest to oldest, from top) – LC, SC, Biconic, Deutsch 1000 (image courtesy theFOA.org).

The table below includes some of the more common connector types:

Acronym

Long-Form Description

Application

FC

Ferrule Connector or Fiber Channel

Datacom, telecom, single-mod lasers, measurement equipment

SC

Subscriber connector

Datacom, telecom

SM

Sub-miniature connector

Industrial lasers, optical spectrometers, military; telecom multimode

LC

Lucent connector or local connector

High-density connections, SFP and SFP+ transceivers, XFP transceivers

ST

Straight-tip connector

Multimode communications

For highest performance (i.e. lowest loss), the tip is then polished to produce a slightly convex surface, called “physical contact” polish. This surface profile means that when the fibers are mated they touch only at their cores, allowing transmission with low loss.

To secure and align the fiber within the connector, the fiber end is embedded in a ferrule made of ceramic (zirconia), stainless alloy or plastic. The ferrule is commonly 2.5 mm in diameter, although 1.25 mm is used in the LC and other connectors.

Fiber-optic adapters

Although fiber-optic connectors get most of the attention, fiber-optic adapters are also a critical part of an optical installation. Fiber-optic adapters enable two connectors to be joined and aligned with minimal losses, no matter whether the connectors are the same type or of different styles (hybrid adapters).

There are numerous adapters to interface between different fiber-optic connectors as can be seen from the samples above.


Figure 2: Hybrid adapter examples (top → bottom): ST → FC, SC → FC, SC → ST (image courtesy theFOA.org).

Adapters are most often used to mate two connectors with ferrules of the same size – 2.5 mm, for example. It is more difficult to align ferrules of different sizes with sufficient precision; hybrid patch cables are more popular for this application.

To minimize losses, the alignment between two fiber-optic cables must be very precise. This is achieved by two primary components – the ferrule within each connector and the alignment sleeve within the adapter. An alignment sleeve in the adapter brings together the ferrules of the two mating connectors so that the optical signal can pass from one fiber to the other with minimal losses.

A comparison of adapter alignment sleeves

Adapter alignment sleeves are made of a variety of materials at various price and performance points.

Polymer sleeves represent the lowest-cost and lowest-performance option. They are generally recommended only for multimode use and limited insertions – 10 or less. When combined with a very hard ceramic ferrule, multiple insertions will scrape off plastic in the form of dust, which forms a film on the end of the fiber and acts as a filter to increase losses. 

Phosphor bronze sleeves are more durable (up to 500 insertions) and work well with ceramic ferrules, but offer lower precision compared to ceramic sleeves. Bronze alignment sleeves are commonly used in multimode applications where precision alignment is not as critical. They are about twice the cost of polymer sleeves.

Zirconia ceramic sleeves are hardest, so offer the highest performance, and are most expensive, up to three times that of polymer. For single-mode applications, zirconia ceramic is required.

Key adapter specifications

Each component in the fiber-optic system contributes to the overall performance. In addition, it’s important that both the adapter and each connector – and all three may be from different manufacturers – adhere to common mechanical standards to ensure precise alignment. The following are the key fiber-optic adapter performance specifications:

Applicable standard – e.g. TIA/EIA FOCIS-3 (see below)

Split-sleeve material – Phosphor bronze, zirconia ceramic or polymer.

Insertion loss – the loss of signal power resulting from the insertion of the adapter into the fiber-optic line; expressed in dB.

Return loss – loss of power in the signal returned or reflected by a refractive index discontinuity in a  fiber-optic line, e.g. due to a mismatch with the terminating load or a device inserted in the line; expressed in dB.

Applicable mechanical standards for connectors and adapters

Various standards have been issued by the Telecommunications Industry Association (TIA) part of the Electronic Industries Alliance (EIA) that cover fiber-optic connectors and adapters.

A FOCIS (Fiber-Optic Connector Intermateability Standard) document is a TIA/EIA component standard to ensure that same-type connectors from different manufacturers will mate together without problems. FOCIS documents have the format TIA-604-XX, where XX refers to the FOCIS number.

According to the TIA, “Intermateability standards define the minimum physical attributes of mating connector components. Fully dimensioned components are not within the scope or intent of FOCIS. The requirements of FOCIS have been selected with the objectives of ensuring that any combination of plugs and adapters conforming to the requirements of FOCIS will mechanically intermate and that intermated connector assemblies will meet their common level of performance. The common level of performance of an intermated connector assembly is the least demanding set of performance requirements in the separate performance specifications of each of the products in the assembly.”

Each FOCIS number covers a different connector type, as shown below.

Standard

Connector Type

FOCIS 1

Biconic

FOCIS 2

ST

FOCIS 3

SC, SC/APC

FOCIS 4

FC, FC,APC

FOCIS 5

MTP/MPO

FOCIS 6

Panduit FJ

FOCIS 7

3M Volition

FOCIS 8

Mini-MAC (Withdrawn)

FOCIS 9

Mini MPO (Withdrawn)

FOCIS 10

Lucent LC, LC/APC

FOCIS 11

Siecor SCDC/SCQC

FOCIS 12

Siecor/Amp MT-RJ

FOCIS 13

SFFSC, SFOC, LX-5

FOCIS 14

SMC-SB

FOCIS 15

MF

FOCIS 16

LSH (E2000)

FOCIS 17

MU

FOCIS 18

1X16 and 2X16 (2013 proposal)

Fiber-optic adapters from Arrow

Arrow offers over 1,600 fiber-optic adapters, connectors, assemblies and tools from many leading manufacturers including TE Connectivity, Molex and Panduit. For example, Molex has a wide range of fiber-optic adapters, including die-cast SC to LC hybrid adapters with EMI shielding, 8-port LC adapters with both phosphor bronze and ceramic sleeves, snap-in ESCON to ST adapters for multi-mode use, and many others.

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.