The Ultimate Pi Week Shopping Guide 2018

게시자

Utilized by engineers and hobbyists alike, the Raspberry Pi 3 is one of the top SBCs (single-board computer) on the market today. From robotics to classic arcade games, this adaptable board from Raspberry Pi Foundation can do practically anything imaginable. Whether brand new or a seasoned pro, there are many exciting and interactive ways that you can dive into the world of possibilities with Raspberry Pi.

JustBoom Amp HAT Kit 

1117_JustBoom_Amp_HAT_Kit

With the JustBoom Amp Hat Kit, you’ll have everything you need to build an impressive audio quality system all in a small package. The kit is a plug-and-play package that is simple to use and setup, meaning no soldering or technical knowledge needed.

You’ll be able to plug in the power cable and connect the kit to a set of passive speakers where you can set up your Max2Play license, making it quick to run and enjoy high quality audio playback within minutes! With the Raspberry Pi GPIO pins still accessible on the Amp Hat, you can easily customize it to fit your project – adding sensors, LEDs, buttons, or anything that will make your project standout.

Common Uses:

  • Multi-room streaming/local audio player
  • Streaming (either from cloud or network storage) high-definition audio
  • Internet radio player with high quality stereo audio
  • Arcade table projects with high quality audio
  • Interactive art projects with audio requirement

Kit Includes:

  • JustBoom Amp HAT
  • Case
  • Raspberry Pi 3
  • Power Supply
  • Max2Play Image

AlphaBot

 1117_AlphaBot_Raspberry_Pi

Have a robotic platform that can do line tracking, avoid obstacles, measure speed, and IR control with the AlphaBot for the Raspberry Pi 3 (Pi not included). The kit comes with the AlphaBot robotic platform mainboard. You can get quickly get started with robotic development that can even include video monitoring via network. With Raspberry Pi open source resources, you will be able to design your own robot for certain activities.

Features:

  • Interfaces with Raspberry Pi and/or Arduino
  • Arduino extend header, supports Arduino Shields
  • Plug-and-play modules (eliminating connecting messy wires) like line tracking, obstacle avoidance, speed measuring, ect.
  • LM298P motor driver with diode protection circuit, meaning more safety
  • LM2596 voltage regulator, providing stable 5V power to the Rapsberry Pi/Arduino
  • TLC1543 AD acquisition chip, allowing the Pi to use analog sensors.
  • Does not include Raspberry Pi or Batteries

Kit Includes:

  • AlphaBot Chassis Kit
  • Tracker Sensor
  • Photo Interrupter Sensor
  • Infrared Proximity Sensor
  • IR Remote Controller

Cupcade 

 1117_Raspberry_Pi_Arcade_Kit

The Cupcade is a Raspberry Pi powered arcade, all in a micro cabinet! Play all the old memorable arcade games in this small package that contains many parts, so be ready to take your time building this awesome mini-arcade. Be sure to have a Raspberry Pi 3, soldering iron, soldering, basic electronic hand tools, and tape ready!

Features:

  • DIY Cupcade enclosure that includes a mono speaker and audio amp
  • Pay old arcade games that you can find online
  • Configure for either vertical or horizontal screen
  • Does not include a Raspberry Pi

Kit Includes:

  • PiTFT Mini Kit
  • 5V 1A USB port power supply
  • USB ‘Noodle’ Cable – A/MicroB – 3ft
  • Laser cut acrylic Cupcade Enclosure
  • 4GB SD/MicroSD Memory Card (Blank)
  • Analog 2-axis Thumb Joystick with Select Button + Breakout Board
  • 2 x 16mm Panel Mount Momentary Pushbutton – Black
  • 2 x 16mm Panel Mount Momentary Pushbutton – Red
  • Arcade/Button Quick-Connect Wire Pair – Set of 10 pairs
  • 8 Ohm 1 Watt Speaker – 3” Diameter
  • Right-Angle 3.5mm Stereo Plug to Pigtail Cable
  • Premium Female/Female Jumper Wires – 40 x 6”
  • Custom Cupcade controller board

Google AIY 

 1117_AIY_Google_Kit

Last year Google released the Google AIY Kit, which uses a Raspberry Pi 3 as its brain (RP3 not included in kit). You can use this kit to create your own Google Assistant and use it with a simple push of a button (or using your own voice). Most of the equipment is included in the kit, but we recommend checking this video out to see how to build it and what you will need!

Features:

  • Built a standalone voice recognition system using the Google Assistant
  • Add voice recognition and natural language processing to Raspberry Pi projects
  • Easy-to-build, no need for soldering
  • Does not include Raspberry Pi

Kit Includes:

  • Voice HAT accessory board
  • Voice HAT microphone board
  • Plastic standoffs
  • 3” speakers (wires attached)
  • Arcade-style push button
  • 4-wire button cable
  • 5-wire daughter board cable
  • External cardboard box
  • Internal cardboard frame

To find more great Raspberry Pi Products check out the Arrow.com Pi Shop!

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.