Arrow Inside the Lab - LTC2380-24

Arrow goes inside the lab with the LTC2380-24 from Analog Devices' Power by Linear.

Welcome to inside the lab with Arrow Electronics.  The web series dedicated the latest in technology and electronics.  Today, we’ll show you Analog Devices' Power by Linear's 24 SAR LTC2380-24.  It consumes a low 28mW of power operating at two mega samples per second, has an integrated digital filter that promises 145dB of dynamic range at 30.5sps.  It has no missing codes a full sampling rate, operates with no latency, and offers low distortions, making it ideal for applications such as seismology, energy exploration, and medical imaging.  We’ll walk you through our demo set up and highlight some of the things we did to maximize the performance using demo kits from Analog Decives' Power by Linear.   

The LCT2380-24 is such a high quality ADC that you need a high quality source to its capabilities.  We’re using the DC1858 to produce two kilohertz sound wave.  This provides a clean signal so we can get what we want.  The source goes to a fully differentiated ampliphier that splits it and provides a common mode voltage that goes in and acts as the wrap over two.  This is how we get a clean, easy to see source.  We then have to worry; about the sample clock for the ADC itself.  We have a demo board for LTC’s dc1216 a low cost low notice 100 MHz clock.  This clock drives the ADC.  It’s a sampling clock so it knows how frequently to sample.  On the DC 2289A you get an optional first order low pass filter.  This also includes a 100 MHz rail to rail input to output that acts as an input buffer to the ADC.  All of this is set up for the AC sampling.  It’s also easy to switch over to DC sampling; we’ll do that in a minute.  It’s just a quick jumper change and you’re good to go. 

We’re going to discuss the output information that I’m getting from PScope. (DEMO) It’s quite impressive.  It has all the parameters, all the harmonics.  You can change the size of the bins and mega samples per second and how you’re going to window it.  It’s a great tool to show the ADC works and all the benefits you can get from the ADC. 

Now we have the DC measurements set up.  We have 10 volts coming into the board, created by our friend Bong at Arrow.  It actually splits it from 10volts down to 2.5 volts.  It cleans as much noise out as possible.  It then goes to our LTC2380 that is set up for DC measurement, then goes to the communication board, which is the DC590B.  As we look here at the laptop we can see that the DC noise is about 75MHz, which is very low.  It shows how quite this ADC can get.  We can also use the Linduino. 

The LTC2380-24 comes in a 16 lead msoft or a 4mm DFM package and is drop in pin compatible with the family of 16, 18, and 20 bit SAR ADC’s.  Allowing designs using these ADC’s to upgrade easily.

All the evaluation boards are available at Analog Devices' Power by Linear.  You can learn more at Arrow.com

 

최신 동영상

죄송합니다. 선택한 필터와 일치하는 결과가 없습니다.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.