How to connect existing smart home devices to Matter

An EDN article by Rob Alexander

With the emergence of Matter comes a wide breadth of opportunities to improve Internet of Things (IoT) connectivity and enable new applications and solutions for years to come. Matter is an application layer that allows different products from different vendors using other technologies to work seamlessly together.

The protocol aims to reduce fragmentation between different manufacturers and enhance interoperability between smart home devices and IoT platforms from different vendors. To achieve this goal, Matter will use Internet Protocol (IP) that provides interoperability between devices to define a standard application layer—regardless of the underlying network protocol.

If IoT companies want to stay ahead of the curve in today’s evolving market, they’ll need in-depth expertise in the underlying Matter IoT wireless protocols, including Bluetooth, Thread, and Wi-Fi. So, how exactly can you achieve Matter interoperability regardless of protocol? The answer may lie in bridging.

What’s bridging and why it’s needed

With a large, existing installation base of non-IP based Zigbee, Z-Wave and other wireless IoT protocols, wireless coexistence is necessary and exceedingly complex. There are currently over 2,100 certified non-IP based smart home products on the market supporting a wide range of applications. With the development of the Matter standard, these devices will need to be bridged to ensure compatibility with the new protocol.

Products using Zigbee or Z-Wave—like Philips Hue bulbs, SmartThings sensors, Ring Alarm system, and Ecobee thermostats—are already on shelves and in homes around the world but are not currently compatible with Matter. In general, connecting Zigbee and Z-Wave devices to Matter will involve updating existing hubs or adding a new bridge that supports the new protocol.

Developers need a way to connect Matter to these devices and bring today’s existing smart home devices into the future, so consumers can enjoy the benefits of Matter with their existing products. Even though some companies may choose to upgrade their end devices in-field if they meet the flash and RAM requirements, it will be wiser for IoT providers to bridge already-existing sensor networks with Matter networks because it will provide users with a more intuitive, easier experience.

Thankfully, a growing number of IoT companies plan to introduce bridging products that will help support both deployed Zigbee/Z-Wave products and the newer Matter products which use Bluetooth Low Energy (LE) for commissioning and run over Thread, Wi-Fi, and Ethernet protocols. Let’s take a closer look at how a Matter bridge works.

How Matter bridge works

A Matter bridge works by extending connectivity to non-Matter IoT devices in a Matter fabric and allows consumers to keep using existing non-Matter devices such as Zigbee and Z-Wave devices together with new Matter devices. The bridge connects to each device using their respective protocols, such as Zigbee, Z-Wave, or Bluetooth, and then translates messages between them into a Matter protocol that they can all understand.

So, when one device sends a message to the other, the bridge intercepts it, translates it into the Matter protocol, and then sends it to the receiving device. The receiving device then translates the message back into its own protocol and acts on it accordingly.

Essentially, the Matter bridge acts as a mediator between smart home devices that use different communication protocols. It enables devices to work together seamlessly, regardless of the protocols they use. This is particularly important for consumers, who may have smart home devices from different manufacturers that use different protocols.

With a Matter bridge, they can connect all their devices to a single network and control them from a single app or platform. The diagram below shows both connectivity between Thread network and Matter fabric as well as Matter to non-Matter networks like Z-Wave/Zigbee using a bridge device.

1123-image-of-matter-bridge-works-diagram
This is how a Matter bridge works by connecting all the devices to a single network.
Source: Silicon Labs

Matter over Thread

To enable connecting to Matter over Thread, many smart home device manufacturers are building border routers that support both Thread and Matter protocols. These devices are designed to act as a router between Thread-based smart home devices and Matter-based devices, allowing them to communicate with each other.

What makes Thread unique to other bridges and hubs is its ability to be built into other devices because it is IP based. IoT providers are building a variety of hardware devices that will act as Matter-compatible Thread border routers like smart home hubs, smart speakers, smart locks, and smart lighting to provide users with seamless interoperability across existing Matter and non-Matter devices.

Overall, any device that supports both Thread and Matter has the potential to act as a border router between the two protocols. With the growing popularity of Matter, we are likely to see an increasing number of devices that support both Thread and Matter.

Furthermore, it is possible to combine Thread Border Router functionality with a Matter Bridge to enable support for Matter Thread and non-Matter devices in a single hub. In fact, some companies are already taking steps to make this a reality. For example, Silicon Labs recently released a fully functional Unify Software Development Kit (SDK), offering bridge solutions for Matter to Zigbee and Matter to Z-Wave, as well connecting to Matter Thread devices.

1123-unify-sdk-Si-Labs
The SDK offers bridge solutions for Matter to Zigbee, Matter to Z-Wave, and Matter to Thread devices.
Source: Silicon Labs

Unify SDK is a software network that simplifies IoT infrastructure development, including application processor-based end products, gateways, hubs, bridges, and access points. Each Unify SDK component implements a Message Queuing Telemetry Transport (MQTT) interface, which is a simple messaging protocol, to the unified language based on Dotdot. As a result, it’s a modular, extendible, lightweight, and well-defined interface for system integration.

Although Unify SDK natively runs on Linux, it is architected for portability. The Unify-Matter bridge application is a part of Unify SDK and is based on CSA’s Matter Bridge Application software. The application receives the Zigbee Cluster Library (ZCL) commands on the Matter protocol interface, translates to Unify Controller Language data model, and publishes to an MQTT interface.

Improving connectivity in future smart homes

By using Thread as the underlying wireless protocol for IoT devices and adding Matter support through border routers, IoT providers are making it easier to create a connected ecosystem of devices that work together. Those devices that do not have native Matter support can still interoperate with Matter through a Matter bridge.

This approach enables consumers to choose from a wider range of devices and manufacturers, while still ensuring compatibility and ease of use. As the industry continues to evolve, we can expect to see even more devices that support both Thread and Matter, making it easier than ever before to create a seamless and connected smart home experience.


ArrowPerks-Loyalty-Program-Signup-banner-EN


最新消息

Sorry, your filter selection returned no results.

请仔细阅读我们近期更改的隐私政策。当按下确认键时,您已了解并同意艾睿电子的隐私政策和用户协议。

本网站需使用cookies以改善用户您的体验并进一步改进我们的网站。此处阅读了解关于网站cookies的使用以及如何禁用cookies。网页cookies和追踪功能或許用于市场分析。当您按下同意按钮,您已经了解并同意在您的设备上接受cookies,并给予网站追踪权限。更多关于如何取消网站cookies及追踪的信息,请点击下方“阅读更多”。尽管同意启用cookies追踪与否取决用户意愿,取消网页cookies及追踪可能导致网站运作或显示异常,亦或导致相关推荐广告减少。

我们尊重您的隐私。请在此阅读我们的隐私政策。