MLCC failsafe strategy: future-proof products for demanding automotive applications

Wasilios Pitharas, Application Engineer at Samsung Electro-Mechanics (SEMCO), explores how the construction of an additional copper epoxy layer, commonly known as soft termination, protects the vital inner ceramic material of an MLCC.

Construction of a standard class II automotive MLCC

Ceramic layers are usually printed with a nickel paste (electrode) and then stacked on top of each other. The capacitance is determined by the ceramic material, the electrode’s arrangement and the number of layers. Subsequently, a copper layer is added to the termination, which connects the electrodes and ensures good conductivity. Compared to other manufacturers, SEMCO MLCCs add an additional copper epoxy layer, commonly known as soft termination. This extra layer acts as a buffer for mechanical stress and protects the more sensitive ceramic against breaking. Finally, a nickel-tin plating is added as last outer layer to avoid oxidation and to ensure solderability.

0421 MLCC failsafe strategy Image1 Standard SEMCO Class II Automotive MLCC

Minimize security risk

Why is the additional protection in the form of a soft termination needed and what happens if the ceramic cracks?

As the insulation resistance between the soft termination layers decreases, the ceramic material creates an insulator as a cavity. But, a short circuit between two opposing layers can occur. Depending on the applied voltage, this can lead to an immense thermal power loss, which can destroy the component and make the entire circuit board inoperative. For this reason, automotive manufacturers create their own quality standards.

For example, VW Group defined the VW80808 standard, which includes the "MLCC failsafe strategy". This strategy aims to minimize the mentioned security risk by setting a guideline of which products can be used in which applications.

If a short-circuit causes a power loss of >2.5W, or if it significantly impairs a system’s function [1], the failsafe strategy must be used. This is particularly the case when battery voltage (terminal 15, 30) is applied directly to the component.

VW’s standard offers four options to keep the failsafe strategy. Out of these, all SEMCO product types use a soft termination layer and are qualified according to AEC-Q200. Option number one can be used in every electric system. The other options are limited to the 12V electric system.

I. Series connection of two mutually orthogonal capacitors

The first option that can be used independently of the electric system voltage is the orthogonal placement of two capacitors in series. Image 2 shows this setup in a simplified circuit diagram.

0421 MLCC failsafe strategy Image2 Orthogonal Setup of two Standard Automotive Capacitors

If one of the two capacitors is placed unfavorably to bending stress, the orthogonal arrangement ensures that a backup capacitor remains intact. Since both capacitors are connected in series, the isolation to ground potential is still given.

II. Series capacitor

A Series or "Flexisafe" capacitor uses the previously demonstrated principle of a series connection of two capacitors in a single component. The opposing layers of different potential are not directly above each other. A “floating” layer connects them.

0421 MLCC failsafe strategy Image3 Series Capacitor

However, the internal structure extremely limits the capacitance value. Compared to the previous solution, the principle of series connection plays a role as well as the reduction of active area.

III. Open Mode Capacitor

If a crack would occur in the red marked "risky" area, it is less likely to end in a short circuit as only layers of the same potential would touch each other due to the shorter electrodes.

0421 MLCC failsafe strategy Image4 Open Mode Capacitor

IV. Capacitor with Soft Termination

The advantages of using a capacitor with soft termination include a higher mechanical resistance and an ideal utilization of the available component dimensions. If the layer structure is identical to a standard component, there is no performance gap.

All SEMCO Automotive Class II capacitors have a soft termination. So, why are standard components without soft termination unsuitable in failsafe applications? The reason is that the use of a component with soft termination is only permitted in VW Group, and if it has been tested according to VW 80808-2 (Appendix A "Qualification of MLCC with soft termination"). This standard requires performing several thermal and mechanical stress tests in a row. The most critical tests are the 5mm bending (“Board Flex”) and the moisture resistance test.

Standard automotive components from SEMCO are also tested according to VW80808-2, but with a bending limit of 3mm. This is above the market standard of 2mm for comparable components. The use for the automotive sector is guaranteed, but not for fail-safe applications. When you talk about soft termination in the market, you usually associate it with 5mm bending strength and the failsafe strategy. Here a differentiated approach must be done for SEMCO. The separate product family “PJ” covers the required 5mm bending strength. The qualification according to VW 80808-2 was performed here with regular criteria.

For low and medium capacitance values, additional layers of the same potential are placed on the top and bottom inside the component’s body. In the case that an MLCC would crack, the risk of a short circuit is reduced extremely, which results in an increased mechanical stability of the complete MLCC.

0421 MLCC failsafe strategy Image5 PJ Series - 5mm Bending

For high capacitance parts, an equivalent construction to the standard articles is used (see Image 1). Since a high capacitance value must be achieved, the space is filled with layers to guarantee stability.

The soft-termination tests according to VW 80808-2 were successfully completed for all actively promoted SEMCO Automotive components.

Downsizing

The trend of miniaturization (downsizing) supports the use of the soft termination option even more. The key to small and safe components is both a robust termination and a fine ceramic powder, which enables a thinner layer structure.

Product inquiries

If you would like to learn more about any of the products mentioned in this article, please reach out to Mr. Mokhtar Marzouk at Mokhtar.marzouk@samsung.com.

Sources:
[1] VW 80808-1: 2015-02, Page 9
[2] VW 80808-2, Appendix A „Qualifikation von MLCC mit Softterminierung“
Image 1: Standard SEMCO Class II Automotive MLCC Samsung Electro-Mechanics (SEMCO)
Image 2: Orthogonal Setup of two Standard Automotive Capacitors Samsung Electro-Mechanics (SEMCO)
Image 3: Series Capacitor Samsung Electro-Mechanics (SEMCO)
Image 4: Open Mode Capacitor Samsung Electro-Mechanics (SEMCO)
Image 5: PJ Series - 5mm Bending Samsung Electro-Mechanics (SEMCO)

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.