Servomotors drive rapid growth of industrial control applications

As a device that indirectly compensates motor speed change, a servo motor is motor that controls the rotation of mechanical components in a servo system. Although the servo motor has been extensively used in industrial control, there is always a more convenient way to quickly design a servo motor control system.

Total solution for servo motor industrial control

A servo motor can accurately control motor rotation speeds and turn voltage signals into torque and rotation speed to drive the controlled object. The rotor of a servo motor is controlled by input signals with a quick response. As an execution component in an automatic control system, the servo motor, characterized by a small mechanical time constant, high linearity, and low starting voltage can convert the received electrical signals into the motor axle’s position shift and angle outputs. Currently, there are alternative current (AC) and direct current (DC) servo motors. When the signal voltage is zero, the servo motor will not rotate, and the rotation speed evenly reduces as the torque increases.

A servo system is an automatic system that can randomly change the output energy, including position, direction, and status, of an object as commanded (specified value). In a motor servo control, sensors are installed on the motor and the controlled object. The detection results will return to the servo amplifier for comparison with the command. Therefore, as a servo motor is controlled by feedback signals, it is different from a stepper motor controlled by input pulse signals.

A servo motor comprises the following three devices: (a) The “commanding device” (controller) that gives motion command; (b) the “controlling device” (servo amplifier) that commands the motion of a servo motor with the signals from the commanding device and the feedback signal; and (c) the “driving, sensing device” that drives an object with the power supplied by the servo amplifier and detects its status.

A motor requires speed feedback in a transmission job. After receiving the speed feedback signal, the controller controls the motor driving mechanism to stabilize rotation speed at the target speed. Conversely, we can select a transmission mode based on the speed. Common speed feedback components include the rotary encoder, Hall effect sensor, and resolver transformer (or simply resolver).

Functionally, although all three above functions can feedback speed, the code disc in encoders breaks easily due to vibration in the absence of higher-level protection. Despite the better resolution, repair frequency is high to affect quality and reliability. The Hall effect sensor is cheap, but its resolution is lower, thus reducing control accuracy. In addition, as magnetism reduces after heating, the Hall effect sensor has a shorter lifespan. As the rotor and the stator of revolver are separated, they are contactless. Together with the brushless design, the revolver has a very high protection level against strong vibration, water and oil contamination, thus delivering a lifespan over decades. In addition, dedicated converter chip decoding can convert output analogue signals into digital signals that can compete with the accuracy of rotary encoders. Therefore, the revolver is an ideal speed feedback component.

Arrow SEED introduces an industrial control solution using the SEED-DBS28377_MI and SEED-DBS28377_CORE. This solution realizes a four-revolver servo motor interface to provide an ideal control platform for the feedback control of revolver servomotors. Based on the latest TI C2000 platforms, by integrating the needs for motor control, industrial automation, and power line communication, Arrow SEED launches this universal, easy to deploy, and fit for secondary development total solution suitable for industries, so as to deliver an excellent control platform for industrial automation by maximizing industrial automation and power line communication.

0517 Servomotors drive rapid growth of industrial control applications_seed image

The SEED-DBS28377_CORE is equipped with the TMS320F28377D MCU and 64MB SDRAM. The SEED-DBS28377_MI is equipped with interfaces including DA, USB, SCI, CAN, Ethernet, motor driver + revolver analogue signal collection + ADC, SD, IoT module, and 10-pin JTAG simulation, LED buttons, and power input.

This control system supports a wide variety of motors: three-phase brushless revolver servo motors that are 24V DC, 6-core, 3-phase, 20-30W wattage, and 3000-4000 rpm. It only needs to connect a motor with the system with the corresponding motor driver board. Power connections can refer to the power source design of TI control board solutions.

As a total solution for product development, apart from controlling servo motors more easily, this solution is equipped with a wide variety of interfaces enabling users to quickly develop IoT products. For any equipment, such as machine tools, printing equipment, packaging equipment, textile equipment, laser processing equipment, robots, automated production equipment, requiring power and asking for high accuracy, this servo motor control solution will be an ideal option for relevant applications.

Arrow Seed Logo

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.