Experts predict an explosion of connected “things” to occur over the next few years. As more things get connected, concerns over data privacy and security will escalate. Utilizing Near Field Communication (NFC) as a communication method can help address some of these concerns.
NFC is the critical link
According to market research, soon more users will access the Internet wirelessly via mobile devices than from wired Ethernet connections. These mobile devices offer several different wireless connectivity options, each with their different strengths and capabilities. But only NFC is specifically designed and engineered to provide zero power operation and maximize privacy, both at a very low cost.
Privacy
NFC by design has a limited field of operation, which prevents data snooping that could occur from a distance. It also requires intent—the application of an NFC-enabled device to an NFC-enabled object—in order to read its memory. This approach is in contrast to protocols such as WiFi, which require radios to broadcast information regardless of intent. The limited field plus other features of the protocol help to ensure that data exchange only occurs with the intended party.
Low power
When communicating between an NFC reader and an NFC transponder (tag), energy harvested from the RF field of the reader powers the tag, enabling connectivity for Internet of Things (IoT) devices without using batteries or power. This energy harvesting feature enables a number of low-power and low-cost applications.
Low cost
Adding a connected NFC tag to an embedded system can establish connectivity to mobile devices at much lower cost than Bluetooth or WiFi approaches. In addition, eliminating the need for a battery in an embedded system can further lower an application’s overall bill of materials.
Comparing wireless protocols
Designers have several choices for connectivity, all with trade-offs (see Table 1). WiFi, ZigBee, and Bluetooth all have different strengths and capabilities. None, however, were specifically defined and engineered to provide zero-power operation and maximize privacy, and do both at very low cost, as NFC does.
Overview
Near Field Communication (NFC) is a short-range, wireless connectivity technology designed to be intuitive. NFC enables simplified transactions, data exchange, pairing, wireless connections, and convenience between two objects when in close proximity to one another (up to 10 cm apart). Because the communication is one-to-one and requires such close proximity, data privacy is more inherent than with other wireless approaches. NFC has three communication modes: Read/Write, Peer-to-Peer, and Card Emulation.
Read/Write mode
In Read/Write mode, an NFC reader/writer (or NFC-enabled mobile phone acting as a traditional contactless reader/writer) reads data from NFC-enabled smart objects and acts upon that information. With an NFC-enabled phone, for example, users can automatically connect to websites via a retrieved URL, send short message service (SMS) texts without typing, obtain coupons, etc., all with only a touch of their device to the object.
Peer-to-Peer mode
In Peer-to-Peer mode, any NFC-enabled reader/writer can communicate to another NFC reader/writer to exchange data with the same advantages of safety, security, intuitiveness, and simplicity inherent in Read/Write mode. In Peer-to-Peer mode, one of the reader/writers behaves as a tag, creating a communication link. For example, two devices (such as smartphones) with readers/writers can communicate with each other.
Card Emulation mode
An NFC device in Card Emulation mode can replace a contactless smartcard, enabling use of NFC- enabled devices within the existing contactless card infrastructure for operations such as ticketing, access control, transit, tollgates and contactless payments. NXP has broad product offerings to support the secure transactions necessary for this mode.
NFC Read/Write mode for embedded systems
Most embedded applications that utilize NFC will use Read/Write mode for the link. In these cases, an NFC-enabled device, such as
a mobile device, will provide the active reader, and the tag will be in the embedded system.
Functionally, a connected NFC tag in an embedded system behaves similarly to a dual port memory. One of the memory ports is accessed wirelessly through an NFC interface. The other port is accessed by the embedded system via an I2C interface.
Through this functionality, data can pass from an external source (e.g., an NFC-enabled mobile device) to the embedded system. Furthermore, because NFC connected tags are passive, they can be read from, or written to, by the external source even when the embedded system is powered off.
Because NFC connected tags function similarly to dual port memories, they facilitate any application that requires data transfer between an embedded system and an external system with an NFC reader/writer, such as an NFC- enabled mobile device.
For any product where adding an elaborate touch display Benefits NXP NFC for embedded applications for extended product features and remote control capability would ruin the aesthetics, add unwelcome cost to the bill of materials, or just simply not fit, NXP’s NTAG I2C chip provides the ideal solution. Using a dual port NTAG I2C chip to provide the conduit between an embedded system’s microcontroller and a user’s NFC- enabled reader/writer device (e.g., phone) allows that device to become an extended graphical display and touch screen user interface for the system.
Benefits:
Removes the cost of a fancy touch display from a product’s bill of materials, replacing it with a much more cost-effective NTAG I2C tag chip
Eliminates the cost of a Bluetooth or WiFi interface Simplifies product design (eliminates need for external buttons and dials) and lowers cost
Enhances security (unauthorized control of products not as accessible)
Consumer intent-driven wireless connectivity addresses privacy concerns
Appliances (White Goods)
Home appliances, such as washing machines, are products where aesthetics are important, size is standardized, and gross margins are moderate. Users want form and function, they like special features, but desire easy operation. The NFC connected tag is a cost-effective way
in which a manufacturer can create one product case to house multiple product variants. Communication with the washing machine is as simple as opening an application on an NFC-enabled mobile device, and tapping that device to the machine control panel. All extended settings become available in one convenient location.
Fitness Tracking Wearable
Fitness tracking bracelets help users set fitness goals and track progress against their goals. By definition, wearable devices must be small, aesthetically pleasing, and easily rechargeable. Displays are limited, and direct control of small wearable devices via tiny mechanical buttons can be difficult. Adding an NFC connected tag chip to the electronics inside a fitness band provides access to a much richer user experience. Touching their phone to the band opens up a user display where users input their goals easily, view their progress, and control backup or upload to the cloud. And, the close proximity requirement of NFC communication protects the user’s private data against unauthorized access by others in the vicinity.
Smart Meter Access
As “Smart Meters” for utility usage tracking become more prevalent, utility companies don’t need to read usage data directly from a meter, so the mechanical or digital readouts are primarily for the user’s information. With an embedded NFC connected tag chip as part of the smart meter design, NFC communication can extend the on-meter displays, and provide additional information for an enriched user experience.
(For example, users could access historical usage profiles or graphs in between monthly billing updates.)
Thermostat Control
Thermostat controller interfaces in commercial settings represent a facilities challenge. To conserve energy and support greater efficiency, most facility managers prefer to keep temperatures within a common, narrow range. Yet sometimes certain rooms are too hot or too cold for comfort. Plus, controls can be confusing, hard to see, difficult to manipulate, or caged behind a mechanical lock box. With an embedded NFC connected tag chip, the control interface becomes a sleek unit with an easy-to-read temperature display. Users tap their NFC-enabled mobile devices to the surface and use the graphical interface for temperature adjustments, daily schedule control, or other extended feature access.
Administrative access to electronics devices
Embedding an NFC connected tag chip into electronic products facilitates controlled access. Users with an NFC-enabled mobile device initiate communication via the NFC interface. Microcontroller software limits access to those with appropriate credentials.
Benefits
Removes the cost of external access control measures, such as mechanical enclosures
Adds convenience, especially when combined with the extended graphical user interface available on any NFC-enabled mobile device
Simplifies product design (eliminates need for external buttons and dials)
Increases access flexibility (remotely granted access possible)
Enhances security (unauthorized control of products not as accessible)
Self-serve maintenance
When an embedded system includes an NFC- connected tag, the system controller can use the internal, nonvolatile memory of the tag to store data such as error codes, serial and model numbers, and warranty information. Power to the electronic product is not necessary in order to retrieve data from the tag memory via an NFC-enabled mobile device. Links stored in memory can even launch instructional videos on a mobile device for enhanced consumer convenience.
Saves time and money
Adds convenience, as consumers have greater control at their fingertips
Reduces new product paper documentation, creating a more ecologically friendly approach 4 Cloud-enabled applications on the mobile device provide context-specific information in response to the information retrieved from the tag
Enhances security (have to be within a limited range to retrieve information)
Firmware update
Any product requiring firmware or data updates benefits from the inclusion of an NFC connected tag chip, because it enables data download capability. The on-chip SRAM permits temporary storage of data during the transfer, enabling the tag chip to act as a modem.
Benefits
Adds convenience, as consumers don’t need cables, disks, or other means of data transfer
Saves bill of material costs for those products that wouldn’t normally require a WiFi or Bluetooth interface for their typical operation
Simplifies designs and improves their aesthetics, because external connectors are unnecessary
Increases access flexibility (the contactless interface supports sealed designs)
Enhances security (have to be within a limited proximity to download information)
Warranty registration
Including an NFC connected tag chip in a product facilitates quick warranty registration through a consumer’s NFC-enabled phone, where contact information is already available. Because the user’s NFC-enabled mobile device already contains their contact information as part of their stored data, filling out a form is a one-step process. The necessary product information (such as serial number, model number, etc.) is readily available in the NFC tag memory. The paired user and product information gets stored in the product to facilitate later access, and also transfers to the cloud for the manufacturer’s records via the mobile device’s cellular or WiFi connection.
Benefits
Increases likelihood of consumers completing warranty registration, now estimated at about 25-30% return rate
Removes cost of processing paper warranty cards
Provides avenue to promote linked products, such as authentic consumable replenishments, creating a new revenue stream
NFC makes wireless pairing and commissioning as easy as tapping an NFC reader/writer against the devices to be connected. An NFC reader/writer can operate as a network credential manager, retrieving credentials from programmed devices and writing those credentials to others to facilitate network connection. Or, an NFC-enabled device can connect itself to a network, by passing access codes to a programmed device for verification. In this case, it operates as both a network node and the network credential manager simultaneously.
Proximity required by NFC offers increased security over longer range, or open credential transmission approaches
User intent-driven approach provides consumers greater control
One-touch approach offers convenience and time savings
Bluetooth pairing
Including NFC capability in Bluetooth designs brings tremendous convenience to consumers by localizing the Bluetooth passcode management function into an NFC-enabled reader/writer.
Benefits
Eliminates the typical pairing steps of searching for Bluetooth devices, manually adding the device once found, and entering passcodes
Enhances the customer experience
Auto power up from deep sleep
Offers increased security (NFC proximity for commissioning versus longer range wireless protocols)
WiFi pairing
Rather than typing in passwords, providing credentials to enable access to a secured WiFi network is as easy as tapping an NFC-enabled device to the router. Transfer of credentials for network extenders requires only one tap against the router to retrieve, and one tap against an extender to program.
Benefits
NFC-enabled devices connect by one-tap against the router
Offers increased security (NFC proximity versus longer range wireless credential broadcast protocols)
Provides consumer convenience
Home automation commissioning
Commission home automation networks more easily through NFC-enabled devices. Users tap NFC- enabled mobile phones on gateways and collect network parameters, which they then pass on to home automation items, creating smart devices.
Fast, accurate commissioning saves time
Convenience to consumer is a key selling point
An NFC tag embedded into a PCB and connected Benefits to the board electronic circuitry via a hardwired serial bus provides a permanent, contactless bridge between the product’s MCU and the outside world. The passive (no power required) operation of NFC tags allows reading/writing of data from/to tag memory via the wireless interface even if the device has no power.
NFC tag’s nonvolatile memory stores configuration data and maintains it without power The NFC tag data is accessible via the wireless interface without disassembling products, or even removing them from their packaging
Product validation
Manufacturers can deactivate electronic products via the NFC interface in the factory, with activation only possible upon authentication at the point of sale. For returns, an NFC-enabled product provides a means of accessing identifying information that validates product authenticity.
Multiple product variants from a single platform
An embedded and connected NFC tag’s memory provides the ability to support zero-power product configuration. Manufacturers create a single platform, and enable or disable features by storing appropriate configuration data in NFC tag memory.
Benefits
Fewer PCB versions lowers manufacturing cost 4 Increases flexibility, because configuration can occur at any point in the manufacturing and distribution channel
Reduces retail inventory by enabling last minute, in-the-box product configuration changes
Return logistics
An NFC connected and embedded tag provides a readily accessible memory (even when the power is off) that can hold information such as the product’s owner, warranty registration information, service records, etc.
More efficient product servicing
Faster return logistics
More effective product maintenance
Saves time and reduces servicing costs
Enables wireless product validation
Provides electronic serialization and error code retrieval
Provides a cost efficient means of deterring counterfeiting, grey market diversion, and distribution channel theft
Protects brands by decreasing chances of consumers unwittingly buying counterfeit goods
Reduces fraudulent returns to the manufacturer
Product personalization
Retailers can use the NFC interface to personalize a product without removing any packaging by writing configuration data to the NFC tag’s memory.
Generates new revenue streams
Differentiates from competitive offerings
When a consumer product has replenishment needs, a consumer might not know exactly which type to purchase or where to find authentic replacements. But when that product contains an NFC tag, a brief pass of their NFC-enabled device over the product can initiate a purchasing cycle for authentic products, and offer a variety of sites from which to purchase the goods. An NFC-enabled product can also optimize product operation upon detection of an authentic part.
Application examples
Refrigerator water filters
Furnace filters
Automatic coffee machine filters
Printer ink cartridges
Espresso machine cleaning products
Pet products (vitamins, pest control, etc.)
Vacuum cleaner bags and filters 4 Carpet cleaner machine solution
Benefits
The consumer can easily retrieve the correct replenishment part information
Retrieval of this information initiates a set of purchasing options for the consumer, and sales opportunities for authentic replacement part manufacturers, by directing the consumer to authentic, pre-approved sponsor URL links
These vendors can also offer incentive coupons to consumers via the same interaction
Manufacturers increase their revenue stream from consumable parts
An NFC reader within the product can help notify consumers of expired consumables and optimize product operation when authentic parts are used NXP offers a comprehensive portfolio of NXP tag ICs covering a broad range of use cases, such as pairing, personalization, user interface, maintenance, authentication, payment, and more.
NTAG 21xF: NFC plus field detect tag chips
The NTAG 21xF series, which includes a field detect output trigger that can act as an electronic product wake-up interrupt, builds upon the NTAG 21x series. Typical NFC applications include data exchange, wireless connection, pairing, and proximity device communication convenience. NXP’s NTAG 21xF series supports these uses and more. The NTAG 21xF series, available in a packaged form compatible with printed circuit board assembly, provides support for gaming, goods and device authentication, Bluetooth/WiFi static pairing, connection handovers, and other embedded electronics applications.
NTAG I2C: NFC, field detect, power harvest, and I2C serial bus
NTAG I2C tag chips have an additional I2C serial bus connection, which further enhances and expands applicable uses. NXP Semiconductors, when still part of Philips, invented the now ubiquitous I2C serial bus—a simple, yet elegant means of communicating between electronic devices with minimal physical traces.
The NFC contactless interface, combined with the I2C serial bus connected interface, enables wireless bidirectional communication between electronics and NFC-enabled devices, even when the electronic device is not powered. In order to make full use of the I2C serial bus interface, the electronic printed circuit board (PCB) usually incorporates the NFC tag. The I2C serial bus interface supports communication with the host PCB microcontroller if the NTAG I2C has an external power supply or when using the power harvesting feature.
Data transfer mode using EEPROM (passive/static mode)
When manufacturers embed the NTAG I2C tag chip into products, users can download information (e.g., manuals, error codes, even links for consumable replenishment) via the RF interface to those products even when they are not receiving power, because the NTAG I2C tag chip acts as a connection between the user’s NFC-enabled mobile device and the sealed and packaged product. With power to the device off, the contactless NFC interface can still operate, receiving data that the NTAG I2C tag chip stores in nonvolatile EEPROM memory. Later, when the device has power, the microprocessor can access the previously written data via the I2C serial bus interface. Similarly, the microprocessor can write data to the EEPROM while powered for later access via the NFC interface whether or not the device has power.
Pass-through mode using SRAM (device-powered mode)
For data transfer after communication has been initiated, the on-chip, 64-byte SRAM preserves EEPROM access limits by supporting a data pass-through option. In this case, data flows from the NFC interface through an SRAM buffer to the I2C serial bus interface or vice versa. The NTAG I2C tag chip operates like a modem when in this mode.
Energy harvesting
The NTAG I2C tag chip’s energy harvesting capability and Field Detect (FD) functions work together to
help support power management. Upon application of the RF field to the antenna, the FD output asserts
low, and the energy harvested by the NTAG I2C tag chip from the RF field is output (VOUT) to a Power Management Unit (PMU) (Figure 14 [1]). The PMU distributes received power to both the NTAG I2C tag chip and the microcontroller (Figure 14 [2]), which allows the I2C bus to become active (Figure 14 [3]), enabling communication. Alternatively, the power harvested by the NTAG I2C tag chip can also be applied directly as a source of power for devices requiring less energy, such as low power microcontrollers, sensors and indicators.
Benefits
Enables waterproofing of devices by alleviating the need for connectors
Permits power transfer in cases where physical connection is difficult (for example, through glass) 4 Eliminates the need for easily misplaced wires or cables
To demonstrate the unique properties of the NTAG I2C tag chip, NXP developed the NFC Explorer Kit, an all-in-one demonstration/development resource for NFC connected tag chips. By including a full complement of hardware and software tools, users can not only investigate the capabilities of the chip through the various demonstrations, but also develop and test their own applications.
NXP’s NFC Explorer Kit supports interactive demonstrations and enables exploration of all NTAG I2C tag chip capabilities for both the hardware and the application developer.
Optionally, the addition of the LPC-Link2 Debugger probe kit allows easy debugging of code ported directly into the NTAG I2C Explorer board, facilitating custom applications.
Optional LPC-Link2 debug probe
The LPC-Link2 debug probe is a low-cost development tool platform for the LPC MCUs (such as the LPC 11U24) including a target board with integrated debug probe plus debug ribbon cable, and supported by an Eclipse-based integrated development environment.