The Everyday Athlete Can Now Benefit from Medical Diagnostics Technology

Athos has created smart athletic clothing based on electromyography (EMG) technology, allowing wearers to closely monitor workout metrics.
게시자

When it comes to working out, amateurs and pros alike struggle to optimize fitness. Sure, a coach can help -- but there’s still potential for human error. Now, a company called Athos has adapted standard medical diagnostic technology to provide real-time analysis and feedback during workouts

The Athos technology, fitted into athletic clothing, can gauge how hard your heart is beating, how efficiently you’re breathing, your muscle load and more, and instantly sends this data via Bluetooth to a designated mobile app. The feedback is designed to keep someone who is exercising on track during the workout, and indicates areas for improvement.

Scaling the Technology

Athos bases its products on electromyography (EMG)—traditionally used to diagnose the causes of nerve or muscle disorders—but in this case used to monitor human systems in action. Special form-fitting clothing incorporate a small signaling device, called the Core, which communicates to the mobile app what you did and how you did it. 

According to Athos’ co-founder and tech wizard Dhananja Jayalath, the greatest challenge to making EMG technology available as an everyday workout tool was scale. Typical EMG monitoring machines are large and costly. The company was able to incorporate the technology into the tiny Core sensing device, which in turn is fitted into athletic wear to monitor particular muscle groups.

Some of the other features of Athos’ technology include:

• The Core device is $199. Custom pants or shirts, with sewn-in pockets for the Core, are $99 each. The mobile app is free.
• Athos sportswear comes in men and women’s versions. They also feature hidden pockets to stash keys and other items.
• The machine-washable garments are form-fitting, and can be worn under other workout clothes such as sweats, if desired.
• The Core is calibrated to each individual. Training goals can be entered into the mobile app, and workout periods or sets are stored for record keeping and later analysis.

Making It Real in the Gym

With the mobile device mounted at eye level, the athlete can view workout loads on particular muscles, indicated by colors. For example, if a left leg muscle reads yellow (indicating only a light load) but the right reads red (the muscle is working to its fullest), an imbalance between the two is indicated. The system also reveals if wrong muscles are being used for a particular activity.



Figure 1: The Athos mobile app. (Source: HiConsumption)

Analysis is Key

The app can indicate in real time even small imbalances in form and strength that might harm the entire muscular system and cause injuries. Once imbalances are taken care of, someone who is working out can engage muscle groups to their fullest, from yellow up to orange and red, as indicated by the app.



Figure 2: Demonstrating workout loads on particular muscles. (Source: Popular Mechanics)

The Athos system may not replace coaches and personal trainers, but it does leverage cutting-edge technology, and cost-effectively, for the everyday exercise enthusiast who is trying to become fitter and healthier. 


최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.