Bulgin Limited
Etiquetas similares
Bulgin industrial market application
Bulgin is widely recognized as a leading manufacturer of environmentally sealed connectors & components. With over 95 years of experience in the industry, Bulgin continues to innovate & develop products & services to cater to its global customer base across a variety of markets.
Tough Times Demand Touch Switches: How to Select the Right Switch for Rugged Applications
The design process can be looked at as a series of choices, making decisions about the approach to be taken and selecting the components needed to complete the design. Some designers may consider selecting the correct switch to be a relatively simple decision. However, with the plethora of types available – even in the specialist rugged category – and the multitude of ways of deploying the switch, it is all too easy to make a less than optimal decision. Picking the wrong switch will have a negative impact on the product or system, whether it is a negative user perception or partial or complete system failure.
Cómo saber cuándo necesita un conector de fibra óptica robusto
Ya sea que esté en la cima de una torre de comunicaciones, en un área de construcción o en el fondo del mar, en la actualidad, la fibra óptica se puede encontrar en cualquier lugar. Esta publicación del blog de Bulgin analiza cómo estos hilos delicados de fibras de vidrio son la forma ideal de transmitir información a través de grandes distancias a la velocidad de la luz; sin embargo, a medida que aumentan las demandas de comunicación en entornos hostiles, también lo hacen los requisitos para conectores de fibra óptica resistentes.