Murata Manufacturing
Étiquettes similaires
High-isolation DC/DC converters enhance the stability and safety of motor operation
In motor applications, the use of inverters or converters for power conversion is essential. Employing a high-isolation DC/DC converter can contribute to enhancing the stability and safety of motor operation, particularly crucial for high-power, high-speed motor systems. This article will introduce you to the relevant technologies of IGBT/MOSFET/SiC/GaN gate driver DC-DC converters and the features of a series of high-isolation DC/DC converters introduced by Murata.
The transformation and innovation brought about by technology in the healthcare industry
In recent years, thanks to advances in electronics and information technology, as well as evolving market demands, technology in healthcare applications has been gradually expanding its capabilities. Beyond intelligent notification, it now includes real-time monitoring, real-time positioning, ventilation calculations, medication calculations, data recording, human-computer interaction, and more. This is driving rapid and robust growth in the healthcare industry. This article will introduce the impact of information and communication technology on the healthcare industry, as well as the diverse and comprehensive healthcare solutions offered by Murata.
Thermistors ensure stable operation of automation equipment
Thermistors are ideal devices for monitoring temperature in electronic products because their resistance can change with temperature variations. Additionally, PTC thermistors can serve as resettable fuses, playing a crucial role in ensuring the safe operation of industrial automation equipment. This article will introduce the development and characteristics of thermistors, as well as related solutions offered by Murata.
Obtenez votre échantillon gratuit de condensateur électrolytique en aluminium polymère de Murata (ECAS)
Les condensateurs de la série ECAS sont massivement utilisés dans des produits tels que l'électronique grand public (PC portables, téléviseurs LCD, consoles de jeu, etc.), les systèmes d'entreprise, l'industrie et les réseaux.
A solution for low-power wide area network smart applications
Apart from indoor smart building applications, for outdoor IoT applications in smart buildings/cities, a different set of requirements is needed. These applications require transmission technologies with longer range, lower power consumption, and often operate on battery power with the need for multi-year battery life. In such cases, Low-Power Wide Area (LPWA) network technologies become the preferred choice for these popular applications. This article will introduce the applications and development of LPWA networks and the related solutions offered by Murata.
Gyroscopes and accelerometers assist in accurately grasping the robot's movement accuracy
The robot must be able to grasp its position and speed of movement in space to ensure its accuracy of movement to perform the actions required, and it needs to rely on gyroscopes and accelerometers to detect angular rates and accelerations of movement. This paper introduces the development and characteristics of gyroscopes and accelerometers, as well as the product characteristics of XYZ-axis gyroscopes and XYZ-axis accelerometers launched by Murata with a high integration of 6 degrees of freedom (DOF).
Full range of gate drive power supply products to meet today's power demands
Power supply is the foundation of all electronic devices, and the gate driver is the key to stably provide power supply for devices. A gate driver is a power amplifier that accepts a low-power input from a controller IC and produces a high-current drive input for the gate of a high-power transistor such as an IGBT or power MOSFET. This article will show you the technical concepts of gate drive power supplies and DC-DC converters, and the functional characteristics of the isolated gate drive power supply product series introduced by Murata.
MEMS inertial sensors, accelerometer and gyro sensors, improve vehicle safety
Accelerometer can be used to detect the acceleration of object and gyroscopes detects angular velocity of objects, and are widely used in various devices such as smart phones. In automotive applications, Inertial sensors are widely used and can greatly improve the stability and safety of vehicles. This article will show you the application and development of Inertial sensors in the automotive field, and the product characteristics and advantages of MEMS gyro sensors introduced by Murata.