Moteurs servo
Étiquettes similaires
Servo Motor vs Stepper Motor: Differences and Advantages
In engineering, perfect and universal solutions don’t exist. Each case requires the designer or engineer to identify and implement the best solution for that project’s task, budget, and requirements. One such area is electrical motors; if your application requires precise control, servo and stepper motors are usually the right components for the task. Both motors perform the same general job — rotating a shaft a specific number of degrees or turns — but they do so differently. Each method also comes with important advantages and disadvantages.
Moteur servo et entraînement servo : solutions d’interconnexion pour l'automatisation
TE Connectivity (TE) est un leader dans le domaine du génie mécanique et industriel et de l'automatisation industrielle. À mesure que se développe l'automatisation, TE fournit des solutions à la fois efficaces, écologiques et viables dans un marché mondialisé. La technologie servo associe compacité, flexibilité et fiabilité pour parvenir à offrir à chaque client des résultats impressionnants.
Servomotors drive rapid growth of industrial control applications
As a device that indirectly compensates motor speed change, a servomotor is motor that controls the rotation of mechanical components in a servo system. Although the servomotor has been extensively used in industrial control, there is always a more convenient way to quickly design a servomotor control system.